Hi,I am Using Freescale MC9S08DZ60 in my project,I want to allow backdoor key access  memory.The example Code is as follows :

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi,I am Using Freescale MC9S08DZ60 in my project,I want to allow backdoor key access  memory.The example Code is as follows :

Jump to solution
1,854 Views
少峰孙
Contributor I

const volatile unsigned char NVPROT_INIT @0X0000FFBD=0XC0;

const volatile unsigned char NVPT_INIT   @0X0000FFBF=0XFC;

const byte NVBACK_KEY0 @0x0000FFB0 = 0xC0;

const byte NVBACK_KEY1 @0x0000FFB1 = 0xC1;

const byte NVBACK_KEY2 @0x0000FFB2 = 0xC2;

const byte NVBACK_KEY3 @0x0000FFB3 = 0xC3;

const byte NVBACK_KEY4 @0x0000FFB4 = 0xC4;

const byte NVBACK_KEY5 @0x0000FFB5 = 0xC5;

const byte NVBACK_KEY6 @0x0000FFB6 = 0xC6;

const byte NVBACK_KEY7 @0x0000FFB7 = 0xC7;

 

#define Program_Byte  PGM[21]=0X20;temp=((unsigned char(*)(unsigned int,unsigned char))(PGM))

volatile unsigned char PGM[59]=

{

0X87,0XC6,0X18,0X25,0XA5,0X10,0X27,0X08,0XC6,0X18,0X25,0XAA,0X10,0XC7,0X18,

0X25,0X9E,0XE6,0X01,0XF7,0XA6,0X20,0XC7,0X18,0X26,0X45,0X18,0X25,0XF6,0XAA,

0X80,0XF7,0X9D,0X9D,0X9D,0X9D,0X45,0X18,0X25,0XF6,0XF7,0XF6,0XA5,0X30,0X27,

0X04,0XA6,0XFF,0X20,0X07,0XC6,0X18,0X25,0XA5,0X40,0X27,0XF9,0X8A,0X81

};

 

Decryption process:

 

DisableInterrupts

FCNFG_KEYACC=1;

temp=Program_Byte(0XFFB0,0XC0);

temp=Program_Byte(0XFFB1,0XC1);

__RESET_WATCHDOG();

temp=Program_Byte(0XFFB2,0XC2);

temp=Program_Byte(0XFFB3,0XC3);

__RESET_WATCHDOG();

temp=Program_Byte(0XFFB4,0XC4);

temp=Program_Byte(0XFFB5,0XC5);

__RESET_WATCHDOG();

temp=Program_Byte(0XFFB6,0XC6);

temp=Program_Byte(0XFFB6,0XC6);

__RESET_WATCHDOG();

FCNFG_KEYACC=0;

EnableInterrupts

I find that is not useful to unsecure the chip.According to the database sheet,I have no idea to unsecure,Looking forward to your help,thank you!

Labels (1)
1 Solution
1,670 Views
kef2
Senior Contributor V

I guess that your program_byte() routine is flash programming byte in flash. You shouldn't use it for backdoor unsecure.You need to write directly to backdoor key locations in flash as if they were RAM. But since flash is not readable while KEYACC is set, you need to manipulate KEYACC and write backdoor locations while executing from RAM or data EEPROM.

Execute this from RAM or data EEPROM:

DisableInterrupts

FCNFG_KEYACC=1;

*(byte*)0xFFB0 = 0xC0;

*(byte*)0xFFB1 = 0xC1;

*(byte*)0xFFB2 = 0xC2;

*(byte*)0xFFB3 = 0xC3;

*(byte*)0xFFB4 = 0xC4;

*(byte*)0xFFB5 = 0xC5;

*(byte*)0xFFB6 = 0xC6;

*(byte*)0xFFB7 = 0xC7;

FCNFG_KEYACC=0;

EnableInterrupts

After executing it, don't forget to start debug session in "Hotplug" mode. Backdoor key unsecure is effective until reset (or power cycle), which is performed by default by most of debuggers.

Regards

Edward

View solution in original post

1 Reply
1,671 Views
kef2
Senior Contributor V

I guess that your program_byte() routine is flash programming byte in flash. You shouldn't use it for backdoor unsecure.You need to write directly to backdoor key locations in flash as if they were RAM. But since flash is not readable while KEYACC is set, you need to manipulate KEYACC and write backdoor locations while executing from RAM or data EEPROM.

Execute this from RAM or data EEPROM:

DisableInterrupts

FCNFG_KEYACC=1;

*(byte*)0xFFB0 = 0xC0;

*(byte*)0xFFB1 = 0xC1;

*(byte*)0xFFB2 = 0xC2;

*(byte*)0xFFB3 = 0xC3;

*(byte*)0xFFB4 = 0xC4;

*(byte*)0xFFB5 = 0xC5;

*(byte*)0xFFB6 = 0xC6;

*(byte*)0xFFB7 = 0xC7;

FCNFG_KEYACC=0;

EnableInterrupts

After executing it, don't forget to start debug session in "Hotplug" mode. Backdoor key unsecure is effective until reset (or power cycle), which is performed by default by most of debuggers.

Regards

Edward