Hi,I am Using Freescale MC9S08DZ60 in my project,I want to allow backdoor key access  memory.The example Code is as follows :

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Hi,I am Using Freescale MC9S08DZ60 in my project,I want to allow backdoor key access  memory.The example Code is as follows :

跳至解决方案
1,268 次查看
少峰孙
Contributor I

const volatile unsigned char NVPROT_INIT @0X0000FFBD=0XC0;

const volatile unsigned char NVPT_INIT   @0X0000FFBF=0XFC;

const byte NVBACK_KEY0 @0x0000FFB0 = 0xC0;

const byte NVBACK_KEY1 @0x0000FFB1 = 0xC1;

const byte NVBACK_KEY2 @0x0000FFB2 = 0xC2;

const byte NVBACK_KEY3 @0x0000FFB3 = 0xC3;

const byte NVBACK_KEY4 @0x0000FFB4 = 0xC4;

const byte NVBACK_KEY5 @0x0000FFB5 = 0xC5;

const byte NVBACK_KEY6 @0x0000FFB6 = 0xC6;

const byte NVBACK_KEY7 @0x0000FFB7 = 0xC7;

 

#define Program_Byte  PGM[21]=0X20;temp=((unsigned char(*)(unsigned int,unsigned char))(PGM))

volatile unsigned char PGM[59]=

{

0X87,0XC6,0X18,0X25,0XA5,0X10,0X27,0X08,0XC6,0X18,0X25,0XAA,0X10,0XC7,0X18,

0X25,0X9E,0XE6,0X01,0XF7,0XA6,0X20,0XC7,0X18,0X26,0X45,0X18,0X25,0XF6,0XAA,

0X80,0XF7,0X9D,0X9D,0X9D,0X9D,0X45,0X18,0X25,0XF6,0XF7,0XF6,0XA5,0X30,0X27,

0X04,0XA6,0XFF,0X20,0X07,0XC6,0X18,0X25,0XA5,0X40,0X27,0XF9,0X8A,0X81

};

 

Decryption process:

 

DisableInterrupts

FCNFG_KEYACC=1;

temp=Program_Byte(0XFFB0,0XC0);

temp=Program_Byte(0XFFB1,0XC1);

__RESET_WATCHDOG();

temp=Program_Byte(0XFFB2,0XC2);

temp=Program_Byte(0XFFB3,0XC3);

__RESET_WATCHDOG();

temp=Program_Byte(0XFFB4,0XC4);

temp=Program_Byte(0XFFB5,0XC5);

__RESET_WATCHDOG();

temp=Program_Byte(0XFFB6,0XC6);

temp=Program_Byte(0XFFB6,0XC6);

__RESET_WATCHDOG();

FCNFG_KEYACC=0;

EnableInterrupts

I find that is not useful to unsecure the chip.According to the database sheet,I have no idea to unsecure,Looking forward to your help,thank you!

标签 (1)
1 解答
1,084 次查看
kef2
Senior Contributor V

I guess that your program_byte() routine is flash programming byte in flash. You shouldn't use it for backdoor unsecure.You need to write directly to backdoor key locations in flash as if they were RAM. But since flash is not readable while KEYACC is set, you need to manipulate KEYACC and write backdoor locations while executing from RAM or data EEPROM.

Execute this from RAM or data EEPROM:

DisableInterrupts

FCNFG_KEYACC=1;

*(byte*)0xFFB0 = 0xC0;

*(byte*)0xFFB1 = 0xC1;

*(byte*)0xFFB2 = 0xC2;

*(byte*)0xFFB3 = 0xC3;

*(byte*)0xFFB4 = 0xC4;

*(byte*)0xFFB5 = 0xC5;

*(byte*)0xFFB6 = 0xC6;

*(byte*)0xFFB7 = 0xC7;

FCNFG_KEYACC=0;

EnableInterrupts

After executing it, don't forget to start debug session in "Hotplug" mode. Backdoor key unsecure is effective until reset (or power cycle), which is performed by default by most of debuggers.

Regards

Edward

在原帖中查看解决方案

1 回复
1,085 次查看
kef2
Senior Contributor V

I guess that your program_byte() routine is flash programming byte in flash. You shouldn't use it for backdoor unsecure.You need to write directly to backdoor key locations in flash as if they were RAM. But since flash is not readable while KEYACC is set, you need to manipulate KEYACC and write backdoor locations while executing from RAM or data EEPROM.

Execute this from RAM or data EEPROM:

DisableInterrupts

FCNFG_KEYACC=1;

*(byte*)0xFFB0 = 0xC0;

*(byte*)0xFFB1 = 0xC1;

*(byte*)0xFFB2 = 0xC2;

*(byte*)0xFFB3 = 0xC3;

*(byte*)0xFFB4 = 0xC4;

*(byte*)0xFFB5 = 0xC5;

*(byte*)0xFFB6 = 0xC6;

*(byte*)0xFFB7 = 0xC7;

FCNFG_KEYACC=0;

EnableInterrupts

After executing it, don't forget to start debug session in "Hotplug" mode. Backdoor key unsecure is effective until reset (or power cycle), which is performed by default by most of debuggers.

Regards

Edward