OpenCL 1.2 Full profile support iMx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenCL 1.2 Full profile support iMx6

3,175 Views
mohamedsarjoond
Contributor III

Hello team,

Does OpenCL1.2 Full profile module is supported in iMx6Q?

How to make use of OpenCVs standard routines(ex: median filter, histogram equalization, cvtColor) with OpenCL 1.1 Embedded Profile.

Please clarify us on this ASAP as its very urgent.

Thanks in advance,

Sarjoondeen.

Labels (3)
0 Kudos
Reply
1 Reply

2,076 Views
art
NXP Employee
NXP Employee

Please refer to the Chapter 5 of the attached document for the detailed information on what of OpenCL is supported in the latest L3.14.52 Linux BSP for i.MX6Q.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply