About calculation of mipi clock in i.MX6DQ.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About calculation of mipi clock in i.MX6DQ.

跳至解决方案
1,781 次查看
keitanagashima
Senior Contributor I

Hi All,

I have a question about mipi clock.

Refer to document in below link.

https://community.freescale.com/docs/DOC-94312#comment-29669

How should you calculate the OV5640's MIPI clock (= 849MHz)?

======

-     mipi_csi2_write(info, 0x00000014, CSI2_PHY_TST_CTRL1);//ov5640 output clk

&

The range and the exact value when ref_clock is 27M are showed as below:

//  800-850MHz  :0x14   //849Mhz

======

Best Regards,

Keita

标签 (6)
0 项奖励
回复
1 解答
1,397 次查看
Yuri
NXP Employee
NXP Employee

Hello, Keita !

  Sorry, there is no detailed information about clock settings (programming
internal MIPI CSI-2 DPHY registers), because of third party agreement.


For some details :

MIPI CSI and IPU questions


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,398 次查看
Yuri
NXP Employee
NXP Employee

Hello, Keita !

  Sorry, there is no detailed information about clock settings (programming
internal MIPI CSI-2 DPHY registers), because of third party agreement.


For some details :

MIPI CSI and IPU questions


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复