Hello,
is there a patch for the freescale Kernel 3.10.17 to made the display no interrupt from uboot to kernel (LCD and LVDS)?
A similar patch is available for Android (JB4.2.2_1.1.0-GA and L3.0.35_4.1.0-GA BSP):
https://community.freescale.com/docs/DOC-98109
Thanks in advance!
Best Regards,
Christoph
Hi Christoph,
You can port boot LOGO from patch for L3.0.35_4.1.0-GA BSP to 3.10.17, the procedure is not difficult , because it is from one u-boot to another u-boot.
Regards,
Weidong
Hi Weidong,
unless I'm wrong you have to patch both u-boot and the kernel.
I think the patches for the kernel are for version 3.0.35 and not for 3.10.17.
The patches won't apply, because the structure of the kernel changed a lot (e.g. board file --> device tree)
Best Regards,
Christoph