Problem to deploy Yocto image with UUU and i.MX8MQ (M8M051)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem to deploy Yocto image with UUU and i.MX8MQ (M8M051)

263 Views
MagVille1205
Contributor II

Hey,

I've been trying to build a Yocto image for my i.MX8MQ (M8M051) board, while following the NXP documentation and Yocto project. I have finally finished compiling the image, but I can't seem to be able to deploy it. For technical reasons, I have to use USB (UUU) to flash the image. Based on the NXP doc :

MagVille1205_3-1743763152043.png

and the files in my  folder ( /imx-yocto-bsp/build-m8m051/tmp/deploy/images/imx8mqevk ), I'm using the followings lines to compile :

MagVille1205_0-1743762503772.png

As you can see, there seems to be a problem with the boot -f imx-boot-imx8mqevk-sd.bin-flash_evk file.

I have a copy of the manufacturer yocto image and his compiles well. So I know the problem isn't drivers, board, cable.... but my image.

I put a screenshot of all the files in my folder, so that you could tell me if i'm using the wrong one....

If anyone has a suggestion or more questions, I'm happy to hear them !

Thanks in advance for the help !

https://www.nxp.com/docs/en/user-guide/RTEDGEYOCTOUG.pdf

https://docs.yoctoproject.org/brief-yoctoprojectqs/index.html

MagVille1205_1-1743762606238.png

MagVille1205_2-1743762637366.png

Tags (2)
0 Kudos
Reply
0 Replies