Booting-IMX8MM-Mini-board-using-V2024-04-version-Yocto-Scarth

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Booting-IMX8MM-Mini-board-using-V2024-04-version-Yocto-Scarth

786件の閲覧回数
Babu_P
Contributor I

Hello NXP,

 

I'm trying to boot the IMX8MM Mini Board using V2024.04 U-boot Version.

I'm facing issue while signing and authentication.

Babu_P_0-1721046445086.png

 

Currently I'm upgrading to the Yocto Zeus ( u-boot v2020.04 version and Linux kernel 5.4.70) to  (Uboot-imx v2024.04 and kernel 6.6.26) Scarthgap.

before this I upgraded to Krikstone u-boot v2022.04  and linux kernel 5.15.70.

I booted the U-boot v2022.04 successfully. while booting kernel i faced below issues

Issue: CSF Header Authentication failed. and some time IVT not found.

In Ubootv2022.04 source code Kernel load address was changed from 0x40480000 to 0x40400000.

Later I changed the Kernel load address to 0x40480000 in u-boot.  Later its booted the kernel.

 

Now i'm trying to boot the u-boot v2024.04 version.

 

I'm using cst-3.3.1.tgz version for signing the image.

 

csf-spl.txt: https://github.com/pullannagari-babu/imx/blob/main/csf-spl.txt

csf-fit.txt : https://github.com/pullannagari-babu/imx/blob/main/csf-fit.csf

csf-linux.txt: https://github.com/pullannagari-babu/imx/blob/main/csf-linux.txt

Zeus uboot-v2022.04  imx-boot.log:

https://github.com/pullannagari-babu/imx/blob/main/v2022.04_zeus-imx-boot.log

Scathgap-Uboot-2024.04 imx-boot.log:

https://github.com/pullannagari-babu/imx/blob/main/v2024.04_scathgap-imx.boot.log

 

 

########################################################

Zeus v2020.04

$ csf-spl.tx

# Authenticate Start Address, Offset, Length and file

    Blocks = 0x7e0fc0 0x0 0x2a600 flash.bin"

                      self           

spl hab block:   0x7e0fc0 0x0 0x2d400  // as per the log

 $ csf-fit.txt

# Authenticate Start Address, Offset, Length and file

Blocks =                    0x401fcdc0    0x57c00       0x1020 flash.bin"    

sld hab block:          0x401fcdc0    0x57c00       0x1020   //as per the log

                                   sld_header_off

csf_offset=$(grep -e "\bcsf_off\b" $TOP_BUILD_DIR/tmp/work/imx8mmevk-poky-linux/imx-boot/1.0-r0/temp/log.do_compile |awk  '{print $2}')

sld_csf_offset=$(grep -e "\bsld_csf_off\b" $TOP_BUILD_DIR/tmp/work/imx8mmevk-poky-linux/imx-boot/1.0-r0/temp/log.do_compile |awk  '{print $2}')

 csf_off                0x2d400

 sld_csf_off            0x58c20

dd if=$WORK_DIR/cst/signed_images/csf-spl.bin of=$WORK_DIR/cst/signed_images/flash_signed.bin seek=$((csf_offset)) bs=1 conv=notrunc

dd if=$WORK_DIR/cst/signed_images/csf-fit.bin of=$WORK_DIR/cst/signed_images/flash_signed.bin seek=$((sld_csf_offset)) bs=1 conv=notrunc

########################################################

Scarthgap v2024.04

cat csf-spl.txt

spl hab block:         0x7e0fc0 0x0 0x30200

csf_off                0x30200

cat csf-fit.txt

sld hab block:         0x401fadc0  0x57c00  0x1020

sld_csf_off            0x58c20

# in v2024.04 version added below block newly for these also need create the csf-fdt.txt file ?

fit-fdt hab block:     0x401fadc0 0x57c00 0x3020           

fit-fdt csf_off        0x5ac20

                                                  

csf_offset=$(grep -e "\bcsf_off\b" $TOP_BUILD_DIR/tmp/work/imx8mmevk-poky-linux/imx-boot/1.0-r0/temp/log.do_compile |awk  '{print $2}')

sld_csf_offset=$(grep -e "\bsld_csf_off\b" $TOP_BUILD_DIR/tmp/work/imx8mmevk-poky-linux/imx-boot/1.0-r0/temp/log.do_compile |awk  '{print $2}')

 csf_off                   0x30200

 sld_csf_off            0x58c20

fit_fdt_csf_off       0x5ac20

 

dd if=$WORK_DIR/cst/signed_images/csf-spl.bin of=$WORK_DIR/cst/signed_images/flash_signed.bin seek=$((csf_offset)) bs=1 conv=notrunc

dd if=$WORK_DIR/cst/signed_images/csf-fit.bin of=$WORK_DIR/cst/signed_images/flash_signed.bin seek=$((sld_csf_offset)) bs=1 conv=notrunc

 

here

spl hab block block correct size how to find it ?

sld hab block: address was modified  0x401fcdc0 to 0x401fadc0.

im not able to boot the v2024.04 what is the correct csf offset to use to sign and authentication.

タグ(2)
0 件の賞賛
返信
0 返答(返信)