i.MXソリューション知識ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Solutions Knowledge Base

ラベル

ディスカッション

ソート順:
Adeneo Embedded adds CSI camera support to their i.MX6 Windows Embedded Compact 7 (WEC7) BSP. Camera interface on the i.MX6 is one of highly requested features among customers and in order to cater to this demand Adeneo Embedded developed a camera driver for CSI interface on WEC7.
記事全体を表示
Adeneo Embedded, a Freescale Connected Proven Partner, continues its commitment in working with Freescale on its i.MX product line. With Freescale’s announcement of the i.MX product roadmap (Freescale i.MX Roadmap blog) and Adeneo Embedded’s latest releases of Operating System BSPs for the i.MX6 platforms, the two companies strengthen further their collaboration and capabilities by bringing best products and services to their customers.   Adeneo Embedded has developed Android, Linux, QNX and Windows Embedded Compact BSPs for a wide range of Freescale’s i.MX products. Adeneo Embedded is the first company to develop the Windows Embedded Compact 2013 BSP on the i.MX6 platforms, supporting SABRE SD Board and SD Platform from Freescale, as well as many different 3 rd party boards including SABRE Lite based platforms and various System On Modules. Adeneo Embedded is also the official i.MX6 training partner of Freescale, jointly conducting about 60+ trainings each year across America and Europe .   Adeneo Embedded is pleased to see Freescale announcing the upcoming i.MX7 and i.MX8 series and will help customers designing products based on these new technologies with a complete portfolio of solutions and services to support the integration of Embedded OS, Middleware and Connected Applications.     About Adeneo Embedded Adeneo Embedded provides system integration, design, support and training services to companies seeking world-class expertise in embedded solutions using high-performance architectures. For over 10 years, Adeneo Embedded has helped clients, in all stages of development; create profitable, feature-rich products that incorporate software and hardware solutions based on Windows Embedded, Windows Phone and Windows 8 operating systems. Close working partnerships with industry-leading silicon and software vendors allow Adeneo Embedded to apply its experience to a wide range of embedded solutions for the automotive, industrial, medical,  multi-media, navigation,  networking, mobile and wireless markets. Adeneo Embedded has a global sales and support network backed by engineering offices in North America and Europe.   © 2013 Adeneo Embedded. All Rights Reserved. All other brands or product names are the property of their respective holders   Further information For more information about Adeneo Embedded competences, products and services around Windows Embedded technologies:   visit Adeneo Embedded dedicated web site                 www.adeneo-embedded.com Adeneo Embedded General sales contact                    sales@adeneo-embedded.com   For a local contact in   Central Europe, contact Michael Heinz                      mheinz@adeneo-embedded.com South&North Europe, contact Jeremy Delicato         jdelicato@adeneo-embedded.com America, please contact Mike Ruiz                            mruiz@adeneo-embedded.com Asia, please contact Vijay Raisinghani                       vraisinghani@adeneo-embedded.com
記事全体を表示
iWave Systems, a Proven Partner of Freescale and certified Silver Partner of Microsoft, proudly announced the availability of Windows Embedded Compact 7 (WEC7) Board Support Package (BSP) for its customers for catering high-end applications in its various skews of i.MX6 Quad, Dual, Dual Lite & Solo Qseven CPU modules. Windows Embedded Compact 7 (WEC7) is one of the real time operating system (RTOS) from Microsoft designed to target enterprise specific solutions which supports multiple CPU architectures like ARM/x86, Silverlight 3.0, Multi touch and 3GB size physical RAM. Windows Embedded Compact 7 BSP together with Freescale i.MX6 multicore based platforms is ideal for various applications like Medical handhelds, industrial controllers, consumer electronics devices and also automotive infotainment systems. iWave’s latest Windows Embedded Compact 7 BSP release supports all the version of i.MX6 Qseven modules named Quad, Dual, Dualite and Solo. The various features supported by the BSP is listed in the below: Eboot boot loader Console UART LVDS port HDMI display PCIex1 lane SD/MMC slot USB Host USB device CAN Port Capacitive touch Camera Analog video input Audio In/out SATA Ethernet I2C ports PWM for backlight OpenGL/VG Graphics Music Player Photo Viewer Video Player Multimedia Codecs Active Sync support Connect & Consumer media Expression blend Adobe Flash 10.1 Hive registry support on SD Silverlight 3.0 Windows Embedded Compact 7 on iWave's i.MX6 Qseven Development Kit Besides the i.MX6 Windows Embedded Compact 7 BSP support, iWave Systems also provides WinCE BSP support for various other Freescale hardware platforms i.MX27, i.MX51 and i.MX53. Windows Embedded Compact 7 BSP for iMX6 Qseven Modules | iWave Systems For more information please contact – mktg@iwavesystems.com
記事全体を表示
This video shows how the Crank Storyboard application framework is well suited to run on our i.MX7 Nitrogen7 board. Demo details This demonstration is based on the following: Nitrogen7 board​​ 800×480 LCD display​ Resistive touch Yocto Jethro release Linux kernel 3.14.52 Crank Software details Crank Software Inc. is an innovator in embedded graphical user interface (GUI) solutions. Their products and services enable R&D teams and UI Designers to quickly and collaboratively develop rich animated user interfaces for resource-constrained embedded. The demo above relies on the Crank Storyboard Engine which is: Multi-platform Supported on Linux, Android, QNX, WindowsCE among others Built for embedded Storyboard Embedded Engine scales from low-end to high-end processors 3D optimized For higher end products embedding a GPU For more information, please visit: https://boundarydevices.com/crank-software-demo-on-nitrogen7/
記事全体を表示
Adeneo's entry for solution of the month in collaboration with Congatec
記事全体を表示
i.CORE RQS M6S/DL/DQ i.Core RQS M6S/DL/D/Q is the latest powerful i.MX6 solution provided by Engicam in micro Q7 format. Equipped with single,dual light,dual or quad Cortex-A9 core and different size of memories The full scalability of modules allows to create multiple products with different performance in a very short time to Market. Features Memories 1GB 64bit DDR3-1066  for i.Core RQS M6Q 512MB 64bit DDR3-1066  for i.Core RQS M6D 512MB 64bit DDR3-800  for i.Core RQS M6DL 256MB 32bit DDR3-800 for i.Core RQS M6S 4 GB e-MMC Graphics and Multimedia 2x LVDS output 1x HDMI output Up to three simultaneous display driving support ( i.Core M6Q/D only) Up to two simultaneous display driving support ( i.Core M6S/DL only) Dual display up to WUXGA (1920x1200) and HD1080 OpenGL/ES 2.x 3D accelerator with OpenCL/EP support and OpenVG1.1 acceleration Multi-format HD1080 video decode and encode Peripherals SD Card interfaces USB OTG HS, USB HS HOST, Uart, I2C, I2S, PCI Express SATA 3Gbps (i.Core M6Q/D only) Ethernet 10/100/1000 On board WiFi option available Dimensions Standard uQ7 http://www.engicam.com/en/products/embedded/som/standard/i-core-rqs-m6s-dl-d-q                
記事全体を表示
英国是大多数留学生向往的留学深造目的地之一,(【联系方式QQ-1252839746】当面临诸多例如:Probation、Withdrawal、Suspension、Dismissal、等学术警告问题的时候,很多学生选择了联系我们修改成绩单达到学分GPA要求或删除学术不良记录重新回到学校。)很多留学生在美国学习后都学到了很多知识,成长为更好的自己。但是,在学习过程中,难免遇到磕磕绊绊,比如:刚来到美国会遇到Culture shock(文化冲突);刚入学会听不懂老师的授课内容;生活上出现各种不可预期的困难;mid-term和final期间没日没夜地复习。历练中,很多学生成功克服困难,顺利完成学业,但也有一部分学生面对过 停学 ( Suspension )的尴尬。不过幸好美国愿意给犯错的学生二次入学的机会,并专门针对停学及开除学生提供一个申请流程,称为 Readmission (再次申请录取)。被停学的学生可以曲线救国,最终成功回到原来的校园。 学生被美国学校停学的理由有很多,例如作弊被抓丶GPA低丶违反校规丶代写代考被发现等等。在达到相应严重程度时,学校会给予学生短则一个季度或一个学期,长则一年甚至两年以上的停学处分。在被停学后,大多数学生都想在停学结束后重新回到原学校。那么学生就会面临 Readmission(重新申请录取/重新接纳)的情况。 T同学是美国某大学大二的学生,在被学校停学后,选择了回国待一年。但是当T同学在结束一年的停学后,提出 Readmission 想要重回学校时,学校却拒绝了T同学的请求,T同学一头雾水。 其实 Readmission 时,需要注意的细节有很多,但是大家往往忽略了这些重要内容。下面我们来详细讲解一下跟原学校申请再次录取的注意事项: 各大学对Readmission要求都不同 首先,学生被 停学 ( Suspension )后,学校对于Readmission有着不同程度的入学要求: 1丶停学期限一到,有的学校是无过多要求,直接颁发新的I-20让学生回到学校,这也是最轻松的Readmission。停学期间,学生需要进行一定的自我反省,并积极调整学习方法和学习知识。 2丶也有一部分的学校对再次申请入学是有要求的,涉及到学生需要在反省后,向学校提交Readmission申请表格及个人陈述,审核通过后,学生才能回到学校。 3丶最难的Readmission是学校要求学生重新入学前进行自我完善和提高,例如进行本学校暑期课程的学习或者在其他机构的学习,证明自己是有继续在原学校读书的能力同时可能会要求提供一些额外的支持材料。 申请时间有限制 学生需要仔细研究学校的开始申请日期和截止日期,并及时提交相关材料。如果错过了申请的时间,学生可能会错过重新入学的学期。T同学就是因为没有注意到截止时间,没有及时提交学校要求的材料,导致Readmission阶段仍需要进行二次申请。 停学期间不要贪图玩耍 建议学生停学期间不要回国。很多学生在国内把停学当作放假,各地游玩儿,在家打游戏,吃喝玩乐。这样极其不利于Readmission的申请,重新回到原学校的机率也会降低。 Readmission申请有风险 并不是所有申请Readmission的学生都会通过。学校对于每一位Readmission的学生都会严格的考量。包括学生停学期间的表现和回国态度,重新入学的提交材料审核等,如被认为不具有继续在原学校读书能力的学生有被拒风险。 当面临诸多例如:Probation、Withdrawal、Suspension、Dismissal、等学术警告问题的时候,很多学生选择了联系我们修改成绩单达到学分GPA要求或删除学术不良记录重新回到学校。【联系方式QQ-1252839746】
記事全体を表示
use AdvancedToolKit1.71 earse NANDFLASH,display error ,why ?      FLASH     K9F2G08U0C-SIB0
記事全体を表示
e-con Systems announces their new System-On-Module aimed for Applications which require higher GPU performance and faster network connectivity. eSOMiMX6PLUS System-On-Module is based on NXP’s QuadPLUS/DualPLUS ARM Cortex™ A9 Processor running up to 1.2GHz, featuring 3 high speed Camera interfaces with support for 13MP Camera and supporting 802.11 ac Wi-Fi network. The eSOMiMX6PLUS at volumes is available at USD79 onwards and samples can be bought from the Webstore. Customers wanting to evaluate thee SOMiMX6PLUS, can do so by ordering the AnkaaPLUS development kit from e-con’s Webstore. The development kit, among other accessories, also includes a13MP camera board, 5MP camera board and 7” LCD panel. 
記事全体を表示
This dual display demo, based on our latest Android Lollipop 5.0 release, shows separate applications on each display. The demo is run on a Nitrogen6x with our two 7″ displays (LVDS Hannstar and RGB Okaya), so it is compatible with all our i.MX6 platforms (BD-SL-i.MX6 (SABRE Lite), Nitrogen6_Lite, Nitrogen6_Max,). For more information please visit http://boundarydevices.com/android-lollipop-dual-display-imx6/
記事全体を表示
Hey guys! Here's Adeneo Embedded's Cube OpenGL demo of the WEC7 Congatec board!   Enjoy !
記事全体を表示
iWave Systems, profoundly known for its genuine embedded solution offerings spanning from SOMs to fully integrated systems announced the availability of Windows Embedded Compact 7 (WEC7) reference BSP for Q7 compatible i.MX6 System-On-Module (SOM) besides the existing Linux 3.0.15 & Android ICS 4.0 BSP versions.
記事全体を表示
The BD-SL-i.MX6 formerly SABRE Lite board is a low cost i.MX6 development platform.  One of the best attributes of the board is the significant software support that is available.  This post introduces Qt5.4 from the QT Company.  The video below shows The Qt Company’s enterprise device creation offering, a Qt-optimized pre-built software stack that lets you immediately get started with prototyping on a real device for embedded Linux and Android development.  The demo is running Qt5.4 and the image is available for the BD-SL-i.MX6 as well as our Nitrogen family of products.  Here is a brief video showing some of the capabilities: The video above showed an image created for embedded Linux, and more specifically, built using tools from The Yocto Project and The Freescale Community BSP. Because of this, your products can leverage the packages provided by those projects, and you can use the Yocto build system to integrate your components and tailor your build. For more details, visit http://qt.io or http://boundarydevices.com/qt-for-device-creation/
記事全体を表示
iWave Systems, one of the early adopters of i.MX6 technology has designed i.MX6 based network switch/router solution. The task involved the design and development of a custom carrier card for our i.MX6 Qseven Module, the carrier card also consists of microcontroller. Together with the i.MX6 Qseven module and carrier card, the solution provides router capabilities. i.MX6 based Router Solution The carrier card was designed by iWave to meet the network Router requirement using iWave’s i.MX6 Qseven SOM. The Wi-Fi modules and GPRS modules (mini PCIe form factor) were interfaced to the PCIe 2.0. With the Gigabit Switch connector, the board supports four RJ45 connectors. Totally, there are six Mini PCIe slots available, accommodating both PCIe and USB signals. Microcontroller, in the carrier card, monitors parameters like voltage levels and power status. It also provides user interface by controlling appropriate LED’s to indicate which mini PCIe module is active. Block Diagram iWave’s i.MX 6 Qseven SOM is connected to the PIC Microcontroller through I2C. Connection is in such a way that iMX6 processor, as a Master and PIC microcontroller, as a Slave. Master and Slave to communicate effectively, iWave has designed a unique customized Communication Protocol in which master (iMX 6) will control the peripherals connected to slave (PIC) through protocol commands. iWave also implemented a software in our Qseven  module that enables the upgrade of the microcontroller firmware. For further information or inquiries please write to mktg@iwavesystems.com or contact our Regional Partners website: www.iwavesystems.com
記事全体を表示
These videos demonstrate an example application of a fully cloud-enabled and location-aware mass transport demo built on Freescale's i.MX5x platform with a HD passenger information display, PCAP touch enabled driver control display, and mobilde device (Android phone) integration. The demo showcases how Android provides the potential of significantly shortening the development cycle and accelerating your time-to-market. The demo is based on the Digi ConnectCore i.MX53 System-on-Module solution and was built using our Embedded Application Development Kit for Android (Gingerbread). Smart Tech for Passenger Buses by Digi International - Design West (ESC) 2012 - YouTube - The ARM video interview at Design West Android Bus Demo - YouTube  - The official Digi video overview Visit www.digiembedded.com for additional information, including a special i.MX53 Android Development Kit kit offer for $199. --- VDC Research Awards Digi Best of Show at Embedded World 2012 for Android Application Development Kit with iDigi Device
記事全体を表示
We introduced a new modular embedded Linux board running a i.MX6 processor as part of our HIO Project, a development effort backed by HABEY to create expandable modular embedded computer building blocks that can be used across the entire product development cycle, from evaluation, development, prototyping to finish product.  This i.MX6 core-board is a fully functional embedded board that is designed to fit in a 2-gang electrical wall outlet box. Its has eight 50-pin female headers on the top and bottom of the board which allows 3-dimensional expansions by adding modules like building Lego bricks. To showcase this Lego-like modular embedded Linux board design, HABEY launched a Kickstarter campagin (http://kck.st/1HroOaW) that features a i.MX6 POE ready 7” modular in-wall touch computer based on the core-board and two other modules with Yocto embedded Linux or Android. For more information on our modular i.MX 6 solutions, please check http://hioproject.org/ and http://www.habeyusa.com/embedded-arm-boards/
記事全体を表示
MYD-JX8MX development board based on NXP i.MX8M quad processors provides powerful multi-media functions including dual displays, dual cameras, high-quality audio, etc. The target applications scale from consumer home audio to industrial building automation and mobile computers requiring high-performance and low-power processors. Highlights: - MYC-JX8MX CPU Module as Controller Board - NXP i.MX 8M Quad Application Processor - 1GB / 2GB LPDDR4, 8GB eMMC Flash, 256Mbit QSPI Flash - RS232, 4 x USB 3.0 Host, 1 x USB 3.0 Host/Device, PCIe 3.0 (x4) NVMe SSD Interface, TF Card Slot - Supports Gigabit Ethernet, WiFi/BT and 4G LTE - 2 x MIPI-CSI, HDMI, 2 x LVDS, MIPI-DSI, Audio Input/Output
記事全体を表示
These sockets require significantly more torque to seat than elastomer sockets.
記事全体を表示
MYIR has released a cost-effective and power-efficient ARM Evaluation Kit (EVK) MYD-IMX28X for Freescale i.MX28 family of multimedia applications processors which has an ARM926EJ-S Core, with speed up to 454 MHz. The board can support running Linux operating systems, which allows developers to use it as an i.MX28 reference platform to quickly start their own design. The board takes full features of the i.MX28 ARM processor and has exposed a comprehensive set of peripherals and connectivity options to make the board suitable for smart gateways, human-machine interfaces (HMIs), handheld devices, scanners, portable medical, experimental education and more other industrial applications. The MYD-IMX28X Development Board is using the MYC-IMX28X CPU module as the heart of the system which is an ARM9-based system-on-module (SOM) integrated with the i.MX28 processor, 128MB DDR2 SDRAM, 256MB Nand Flash and Ethernet PHY. It is connected to the base board through two 1.27mm pitch 80-pin connectors. The base board has extended many peripherals and interfaces through headers and connectors, featuring 1 x RS232, 1, Debug, 2 x USB ports, up to 2 x Ethernet, 1 x CAN, 1 x RS485, TF, Audio, LCD, JTAG, etc. MYD-IMX28X Development Board MYC-IMX28X CPU Module MYIR offers the board with Freescale i.MX283 or i.MX287 ARM9 CPU by default; user can integrate a different MYC-IMX28X CPU module on the same base board, thus making two variants of i.MX28 evaluation boards. MYD-IMX283 Development Board – with MYC-IMX283 CPU Module for Freescale i.MX283 MYD-IMX287 Development Board – with MYC-IMX287 CPU Module for Freescale i.MX287 The MYD-IMX283 and MYD-IMX287 boards only have a few differences as described in below table: Model MYD-IMX283 MYD-IMX287 Processor i.MX283 i.MX287 CAN 0 2 Ethernet 1 2 The MYD-IMX28X board comes with Linux2.6.35 software packages, detailed documents, necessary cable accessories as well as optional 4.3- and 7-inch LCD (with touch screen) to provide a complete Freescale i.MX28 starter kit and enable a quickly start of evaluation of i.MX28 family applications processors.
記事全体を表示