i.MXソリューション知識ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX Solutions Knowledge Base

ラベル

ディスカッション

ソート順:
Added by Marsha Chang on April 29, 2011 at 4:56pm
記事全体を表示
Unboxing MYD-C8MMX Dev Kit Based on NXP i MX 8M mini A53 Quad Processor The MYD-C8MMX development board is using the i.MX 8M Mini Quad Processor which is among NXP i.MX 8M mini family of applications processors and includes a 1.8GHz quad Cortex-A53 core plus a 400MHz Cortex-M4 core. The MYC-C8MMX CPU Module provides an outstanding embedded solution for Home and Building Control, IOV, Industrial and Medical Instruments, Human Machine Interface (HMI) and more other general purpose industrial and IoT applications which require optimized power consumption while maintaining high-performance.performance and low-power processors. For more information: http://www.myirtech.com/list.asp?id=618 http://www.myirtech.com/list.asp?id=617
記事全体を表示
iWave Systems, AI/ML demo shows a low power smart door running eIQ heterogeneously on NXP i.MX 8M Mini Development kit. The demo application is built around the Django framework running on the board. In addition to face recognition, the MPUs are able to run a Django server to manage the user’s database, a QT5 application for the graphical interface, and perform training on the edge.
記事全体を表示
The complete tutorial / FAQs are uploaded to http://www.myirtech.com/faq.asp?selec. The tutorial / FAQs are based on MYIR’s NXP i.MX6UL/6ULL series products but are also applicable to similar products from other companies. MYIR hopes these are useful to you. MYIR’s NXP i.MX6UL/6ULL series products: http://www.myirtech.com/nxpseries.asp MYS-6ULX Single Board Computer MYD-Y6ULX Development Board (MYC-Y6ULX CPU Module as core board) MYD-Y6ULX-HMI Development Board (MYC-Y6ULX CPU Module as core board) MYD-Y6ULX-CHMI Display Panel
記事全体を表示
MYD-JX8MX development board based on NXP i.MX8M quad processors provides powerful multi-media functions including dual displays, dual cameras, high-quality audio, etc. The target applications scale from consumer home audio to industrial building automation and mobile computers requiring high-performance and low-power processors. Highlights: - MYC-JX8MX CPU Module as Controller Board - NXP i.MX 8M Quad Application Processor - 1GB / 2GB LPDDR4, 8GB eMMC Flash, 256Mbit QSPI Flash - RS232, 4 x USB 3.0 Host, 1 x USB 3.0 Host/Device, PCIe 3.0 (x4) NVMe SSD Interface, TF Card Slot - Supports Gigabit Ethernet, WiFi/BT and 4G LTE - 2 x MIPI-CSI, HDMI, 2 x LVDS, MIPI-DSI, Audio Input/Output
記事全体を表示
In this demo we are using an OpenCL FFT algorithm to sample audio input from either a wave file or line input and display the frequency bands using OpenVG
記事全体を表示
Watch the demo of Color Segmentation using e-CAM130_iMX8 - 13MP Autofocus Camera Board for i.MX8. e-CAM130_iMX8 is a 13MP 4-lane MIPI CSI-2 autofocus color camera board for i.MX8 family of processors. The e-CAM130_iMX8 camera board is interfaced directly to the CSI-2 MIPI interface on the Variscite's DART-MX8M Evaluation kit (VAR-DVK-DT8M). The iHDR (interlaced High Dynamic Range) support helps to capture good quality images in both high and low illumination. e-CAM130_iMX8 also comes with a high-performance Image Signal Processor (ISP) that performs all the Auto functions (autofocus, auto white balance, auto exposure control).
記事全体を表示
Added by Ji Jian Feng on November 2, 2011 at 10:01pm This is one demo dual display with two different 720P video contents.
記事全体を表示
Are you looking to build a 3D video streaming & recording system that can be used in Stereo Dental Cameras, Obstacle Detection in Robotics, 3D Virtual tours, etc. Look no further, watch this demo of 3D video streaming & recording using Meissa, eSOMiMX6-micro RDK & Dual Cameras. eSOMiMX6-micro is a high performance micro system on module based on NXP/Freescale i.MX6 Quad/Dual Core ARM® Cortex™-A9 in an ultra-small form factor of 54mm x 20mm with just 10mA in suspend current. eSOMiMX6-micro System on Module also supports Wireless LAN and Bluetooth module. OS support – Linux, Android Marshmallow* (* – Under Development). Meissa, the powerful evaluation kit has the smallest carrier board in the industry; it’s just the size of a credit card. Try it and let us know your feedback.
記事全体を表示
The MEasy HMI developed by MYIR is a set of human-machine interfaces which contains a local HMI based on QT5 and a Web HMI based on Python2 back-end and HTML5 front-end. It runs on development boards with LCD, touch panel, Ethernet and so on. The dependency software includes dbus, connman and QT5 applications, python, tornado and other components. The video gives a demonstration on how to use the examples in MEasy HMI on MYIR's MYD-Y6ULX development board. It also applies to MYIR's MYS-6ULX Single Board Computer.
記事全体を表示
The video gives an introduction of MYIR's MYS-6ULX Single Board Computer which is powered by 528MHz NXP https://community.nxp.com/tags#/?tags=imx%206ul / https://community.nxp.com/tags#/?tags=imx6ull ARM # Processor, specially designed for Industry 4.0 (Industrie 4.0) and Internet of Things (https://community.nxp.com/tags#/?tags=iot%3B) applications. More information can be found at MYIR's website: http://www.myirtech.com/list.asp?id=561                               MYS-6ULX Single Board Computer                       A Complete Embedded System based on NXP i.MX 6UL/6ULL Solution
記事全体を表示
This 1-minute video highlights Windows Embedded Compact 2013 running on the Device Solutions Opal i.MX53 Development Kit.  This new version has many performance and productivity enhancements over Windows Embedded Compact 7.  The port was done by Guruce.com.
記事全体を表示
MYIR launches a 7-inch HMI display panel with capacitive touch screen, the MYD-Y6ULX-CHMI, which runs Linux on NXP’s i.MX6 ULL ARM Cortex-A7 processor, is specially designed for HMI system like POS, intelligent access control and more other applications. It provides many peripheral interfaces and much software resources. Know more at MYD-Y6ULX-CHMI | 7-inch HMI Display Solution based on NXP i.MX 6UL/6ULL-Welcome to MYIR 
記事全体を表示
The MYS-6ULX Single Board Computer is powered by 528MHz NXP i.MX 6UltraLite / 6ULL ARM Cortex-A7 Processor, with 256MB DDR3, 256MB Nand Flash on board. This video briefly introduced the features and peripherals on the IoT board and IND board. Know more at http://www.myirtech.com/list.asp?id=561
記事全体を表示
MEasy HMI QT Demo on MYIR's MYD-6ULX development boards. This demo applied to NXP i.MX6UL series development boards of MYIR currently. Welcome to visit our website www.myirtech.com.
記事全体を表示
The complete tutorial / FAQs are uploaded to http://www.myirtech.com/faq.asp?selectm=class&anclassid=6&nclassid=90  The tutorial / FAQs are based on MYIR’s NXP i.MX6UL/6ULL series products but are also applicable to similar products from other companies. MYIR hopes these are useful to you. MYIR’s NXP i.MX6UL/6ULL series products:  MYS-6ULX Single Board Computer MYD-Y6ULX Development Board (MYC-Y6ULX CPU Module as core board) MYD-Y6ULX-HMI Development Board (MYC-Y6ULX CPU Module as core board) MYD-Y6ULX-CHMI Display Panel How to connect Ubuntu to the Internet? Run Oracle VM VirtualBox (this is what I am using, you may use other VirtualBox). Open the settings in the supervisor, choose network, enable network connection, connection type: bridge network card, the name of the interface: Select by actual occurrence. If you want ubuntu to use fixed IP, you may set it up in “Ubuntu/etc/network/interface”. Reference: # interfaces(5) file used by ifup(8) and ifdown(8) auto lo iface lo inet loopback auto enp0s3 iface enp0s3 inet static address 192.168.30.109 netmask 255.255.255.0 getway 192.168.30.1   How to transfer files between Windows PC and the development board? The board and PC should be connected to the same network. Install tftpd64.exe software on the PC. Current Directory, choose the path to upload files. Server interface, choose the IP of PC. Execute “tftp 192.168.1.153 -g -r test.sh” in Xshell when downloading files to the board. Execute “tftp 192.168.1.153 -p -r test.sh” when upload files from the board to PC. 3-3-1 tftpd64 Server configuration How to transfer files between Ubuntu and the development board? The board and Ubuntu should be connected to the same network. Execute scp file to transfer files: “scp -r /home/roy/rs485 [email protected]:/home/root”. Tips: this command means copy folder ubuntu/home/roy/rs485 to directory /home/root of board with IP 192.168.1.223.
記事全体を表示
MYIR launches a 7-inch HMI display panel with capacitive touch screen, the MYD-Y6ULX-CHMI, which runs Linux on NXP’s i.MX6 ULL ARM Cortex-A7 processor, is specially designed for HMI system like POS, intelligent access control and more other applications. It provides many peripheral interfaces and much software resources. Know more at MYD-Y6ULX-CHMI | 7-inch HMI Display Solution based on NXP i.MX 6UL/6ULL-Welcome to MYIR 
記事全体を表示
e-con Systems launches the 13MP Autofocus 4-lane MIPI camera board for NXP i.MX6. This camera is based on 1/3.2" AR1335 CMOS image sensor with advanced 1.1µm pixel BSI technology from ON Semiconductor® and an integrated high-performance image signal processor (ISP) that performs all the Auto functions (Auto White Balance, Auto Exposure control). Target Applications Kiosk Documents Reader/Scanner Unmanned Aerial Vehicles (UAVs) Autonomous Robotic Systems Mobile Medical Imaging Intelligent Video Analytics (IVA) Features Benefits Advanced 1.1µm pixel BSI technology Delivers superior low-light image quality and produces accurate color reproduction 1080p @80 fps - YUV422 High quality HD video playback Interlaced High Dynamic Range (iHDR) Allows to capture clear images in both extreme lighting conditions Pan Tilt Digital Zoom(Upto 8x) Allows to get a closer view of far-away objects Autofocus Allows users to reliably and easily maintain sharp focus on subjects as they move throughout the frame
記事全体を表示
The video provides an interesting demo to enable customers to experience Amazon Alexa Voice Service on MYIR's MYS-6ULX Single Board Computer which is based on NXP's i.MX 6UL/6ULL ARM Cortex-A7 processor.
記事全体を表示
Toradex displayed the new member of its System on Module (SOM) product line based on the NXP® i.MX 7 series applications processors at the Embedded World 2016 - Colibri iMX7D and Colibri iMX7S. The Colibri iMX7S and Colibri iMX7D are SODIMM-sized SOMs based on NXP® i.MX 7Solo and NXP/Freescale i.MX 7Dual SoCs respectively. These SoCs support asymmetric and heterogeneous multi-core processing. Real-time applications are executed on the ARM® Cortex®-A4 and the user-generated applications run on ARM Cortex-A7. Learn more about Colibri i.MX 7 System on Module here.
記事全体を表示