imx-rt boot pin configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx-rt boot pin configuration

Jump to solution
3,614 Views
martinribelotta
Contributor I

Hello. I'm starting a development of imx-rt1021 board using as reference the MIMXRT1020HDUG (Hardware Development Guide), the reference manual (IMXRT1020RM)

In IMXRT1020RM, page 292, section 8.4.2 the table 8-4 specifies this pin bootstrap configuration:

pastedImage_1.png

But, in the datasheet (IMXRT1020CEC), page 72, section 5.1, the table 66 is:

pastedImage_2.png

This is consistent with page 8 of hardware reference manual (MIMXRT1020HDUG), Figure 2:

pastedImage_3.png

And the MIMXRT1020-EVK implementation (Sheet 14)

In concret. The BOOT[1:0] is from GPIO_EMC[17:16] or GPIO_AD_B0_[04:03]?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,368 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Martin,

The internal revision concluded that Table 8-4 of the Reference Manual is a mistake. Thanks a lot for your feedback reporting this issue.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
3,369 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Martin,

The internal revision concluded that Table 8-4 of the Reference Manual is a mistake. Thanks a lot for your feedback reporting this issue.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,368 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Martin,

According with the table of i.MX RT1020 Reference Manual section 4.1.1 “Muxing Options”, the boot select pins are also mapped to GPIO_EMC pins, so it seems to be a typo on Table 8-4.

I have reported this issue, thanks a lot for your feedback. I will post an additional reply when confirming the correct information.


Hope this will be useful for you.
Best regards!
/Carlos

0 Kudos
Reply