iMXRT1064 SWD programming from an external microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

iMXRT1064 SWD programming from an external microcontroller

932件の閲覧回数
etronic_arg
Contributor III

Hi,

I just want to program the internal FlexSPI flash of the iMXRT1064 from an external microcontroller via SWD interface using GPIOs.

I managed to flash a Kinetis K64F from another K64F using 4 GPIO pins connected to a SWD interface (SWDIO, SWDCLK, RESET, GND).

1. Is that possible?
2. Should I only change the programming algorithm?
3. Where can I get the programming algorithm for the iMXRT1064?

Thanks

0 件の賞賛
返信
1 返信

905件の閲覧回数
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @etronic_arg ,

Thanks for your interest in NXP MIMXRT series!

From your description, this application scenario appears to be an offline programmer? Although we have not provided a direct example, this should be possible. One question is, if the SWD is emulated using GPIOs, will the rate be slower? In addition, a previous customer put the RT MCU on the slave side into serial download mode by using the MCU as the host and wrote image in serial download mode. There should be an advantage in speed in this way, and it is also recommended that you consider it.

Best regards,
Gavin

0 件の賞賛
返信