Hi
in table 5-9 there is no definition for booting woth LPSPI. Register 0x450[7:0]???
I can select the LPSPI chipselect register 0x6D0, but how can i select the boot device for LPSPI,
as described in chapter 8-2
The boot ROM supports these boot devices:
• Serial NOR Flash via FlexSPI
• Serial NAND Flash via FlexSPI
• Parallel NOR Flash via SEMC
• RAWNAND Flash via SEMC
• SD/MMC
• SPI NOR/EEPROM via LPSPI