What are the exact bootmode/pins settings for booting via LPSPI?
in the TRM table 8-8 there is no entry about this.
Above there stands
The chip supports these boot flash devices
Serial NOR/EEPROM boot via LPSPI
Solved! Go to Solution.
Hi Christian
pinmux settings are given in Table 8-1. ROM Bootloader Peripheral PinMux
i.MX RT1050 Processor Reference Manual
Boot mode only using fuse mode as shows Table 8-35 (there is no GPIO override mode),
fuse selections are given in Table 5-9. Fusemap Descriptions i.MX RT1050 Processor
Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
in table 5-9 there is no definition for booting woth LPSPI. Register 0x450[7:0]???
I can select the LPSPI chipselect register 0x6D0, but how can i select the boot device for LPSPI,
as described in chapter 8-2
The boot ROM supports these boot devices:
• Serial NOR Flash via FlexSPI
• Serial NAND Flash via FlexSPI
• Parallel NOR Flash via SEMC
• RAWNAND Flash via SEMC
• SD/MMC
• SPI NOR/EEPROM via LPSPI
boot ROM uses it as recovery device using one of the LPSPI ports,
please check description in sect.8.10 Recovery devices
Best regards
igor
OK, thanx, that info helps.