i.MX get microcontroller type

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX get microcontroller type

跳至解决方案
1,775 次查看
Litmus1446
Contributor I

Is there any way to determine the microcontroller type, not family or UID, by reading particular register? I would like to separate between i.MX RT1062 and i.MX RT 1064 while being in ROM bootloader using sdphost.

 

0 项奖励
回复
1 解答
1,745 次查看
Ramon_Vega
NXP TechSupport
NXP TechSupport

Dear @Litmus1446 ,

Thanks so much for your patience, the i.MX RT106x don't have a standard register that identify the part.

but one difference is the 4MB that we have in the internal flash for i.MX RT 1064. Also considering a default XIP memory setup, is to identify if code is being executed at 0x6000_xxxx (i.MX RT1060) or at 0x7000_xxxx (i.MX RT1064).

please see this topic for more information Device Identification Register - NXP Community

I hope this information help you!

Kind regards 

-Ramon.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,746 次查看
Ramon_Vega
NXP TechSupport
NXP TechSupport

Dear @Litmus1446 ,

Thanks so much for your patience, the i.MX RT106x don't have a standard register that identify the part.

but one difference is the 4MB that we have in the internal flash for i.MX RT 1064. Also considering a default XIP memory setup, is to identify if code is being executed at 0x6000_xxxx (i.MX RT1060) or at 0x7000_xxxx (i.MX RT1064).

please see this topic for more information Device Identification Register - NXP Community

I hope this information help you!

Kind regards 

-Ramon.

0 项奖励
回复