Trying to enable SSC on RT1170 EVK with MCUXpresso.
Ref: AN12879
Steps:
1. Base project: SDK Example evkmimxrt1170_semc_cm7
2. Using IDE to config SSC
3. Boot failed
4. Sometimes can boot normally (~ 1/50)
Any step I missed?
Regards
Seen
Solved! Go to Solution.
Hi @SeenFan ,
This is because RT1170 FlexSPI use PLL2 as clock source when use default configure. When you change PLL2 frequency, FlexSPI may fail to get next instruction. To resolve this, you can put fsl_clock.c to SRAM. Please refer to my demo code.
Regards,
Jing
Hi @SeenFan ,
This is because RT1170 FlexSPI use PLL2 as clock source when use default configure. When you change PLL2 frequency, FlexSPI may fail to get next instruction. To resolve this, you can put fsl_clock.c to SRAM. Please refer to my demo code.
Regards,
Jing
Hi Jin,
If I want to locate and run program on SDRAM.
What I need to pay attention to?
Regards
Seen
Hi @SeenFan ,
SDRAM can be initialized by DCD and boot ROM. Then boot ROM will copy your application code to SDRAM. I think the most important thing is the cache problem. You can refer to these link.
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/How-to-move-CM4-core-project-to-SDRAM-in-RT1176...
2.debug in sdram
https://community.nxp.com/t5/MCUXpresso-IDE/Running-and-debugging-program-in-SDRAM/m-p/1405167
3.Using NonCached Memory on i.MXRT
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-NonCached-Memory-on-i-MXRT/ta-p/1183369
Regards,
Jing
Hi Jing,
It works. Thanks a lot.
Regards
Seen