Hello NXP team,
I think I found a potential bug in the code which configure SEMC for i.MX RT1170.
Could you review your source code?
Assumption of hardware where this code runs:
- Externa SRAM is used
- Address A8 pin operates as chip select
Here is snippet of code from SEMC_ConfigureSRAMWithChipSelection in "fsl_secm.c" for i.MX RT1170.
Line#777~789
uint32_t muxCe = (config->cePinMux == kSEMC_MUXRDY) ?
(SEMC_IOCR_PSRAM_CE - 1U) :
((config->cePinMux == kSEMC_MUXA8) ? SEMC_IOCR_PSRAM_CE_A8 : SEMC_IOCR_PSRAM_CE);
I think there should be "#if def" like other part in this function.
For example, here is code from line#855.
#if defined(FSL_FEATURE_SEMC_SUPPORT_SRAM_COUNT) && (FSL_FEATURE_SEMC_SUPPORT_SRAM_COUNT > 0x01U)
case kSEMC_SRAM_CS1:
base->BR9 = tempBRVal;
break;
case kSEMC_SRAM_CS2:
base->BR10 = tempBRVal;
break;
case kSEMC_SRAM_CS3:
base->BR11 = tempBRVal;
break;
#endif /* FSL_FEATURE_SEMC_SUPPORT_SRAM_COUNT */
Otherwise, muxCe is set to wrong setting that is expected for other i.MXRT such as 1060.
Regards,
Norihiro Michigami
AVNET
解決済! 解決策の投稿を見る。
Hi @Norihiro ,
Yes, you are correct. This code is for RT1060 but not fit for RT1170. Their registers are different here. I'll report this error.
Best regards,
Jing
So - has this been fixed yet? I just hit it today after several hours wondering why my 2 CS pins were not operating correctly. I downloaded the SDK recently and fsl_semc.c is still dated 2020.
Hi @Norihiro ,
Yes, you are correct. This code is for RT1060 but not fit for RT1170. Their registers are different here. I'll report this error.
Best regards,
Jing
Hello Jing,
Thank you for checking this report.
I understand that NXP keeps fixing known bugs on SDK.
Can I find any notification once this error gets fixed by
NXP through release note of SDK or this thread?
Regards,
Norihiro Michigami
AVNET
Hi @Norihiro ,
Yes, this bug will be fixed in next release. It will be note in release note.
Regards,
Jing