i.MX RT1024 with an external SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT1024 with an external SDRAM

Jump to solution
1,545 Views
Jigs
Contributor I

I want use the i.MX RT1024 with an external 64MB SDRAM. As per the datasheet it supports 8/16-bit SDRAM External memory interfaces. Which mode is better from performance perspective and how ? Please let me know if there is any link/reference to go through for this details. Thanks

Labels (1)
0 Kudos
Reply
1 Solution
1,498 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Jigs,

The usage between 8/16-bit SDRAM could have the following differences:

  • 8 bit SDRAM means less data bus lines, while 16 bit SDRAM means more data bus width which usually refers to a faster bus and higher transfer rate.
  • 16 bit SDRAM could transmit more data in parallel (as it has more bus lines) than an 8 bit SDRAM in one transfer.

We share you an interesting application note relating with the performance optimization of the i.MX RT Series, that could be useful to the topic: AN12437: i.MX RT Series Performance Optimization – Application Note.

Finally, we share some community post using 8bit SDRAM:

Best regards, Raul.

View solution in original post

0 Kudos
Reply
2 Replies
1,499 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Jigs,

The usage between 8/16-bit SDRAM could have the following differences:

  • 8 bit SDRAM means less data bus lines, while 16 bit SDRAM means more data bus width which usually refers to a faster bus and higher transfer rate.
  • 16 bit SDRAM could transmit more data in parallel (as it has more bus lines) than an 8 bit SDRAM in one transfer.

We share you an interesting application note relating with the performance optimization of the i.MX RT Series, that could be useful to the topic: AN12437: i.MX RT Series Performance Optimization – Application Note.

Finally, we share some community post using 8bit SDRAM:

Best regards, Raul.

0 Kudos
Reply
1,485 Views
Jigs
Contributor I

Thank you @RaRo . Really appreciate your detail explanation on this.

0 Kudos
Reply