i.MX RT cpu family USB OTG dual role

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX RT cpu family USB OTG dual role

ソリューションへジャンプ
1,667件の閲覧回数
uwe_strempel
Contributor I

Hi,

can the i.MX RT cpu family (106x/105x/117x etc.) run usb otg dual role (host/device) at same time?

Best regards

Uwe

0 件の賞賛
返信
1 解決策
1,659件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The HS USBs can be used as device or host (and change between the two roles via OTG protocol). One USB interface can never be used as both host or device at the same time.

On devices with two HS USB controllers one can be host and the other device (or both device or both host).

The following shows dual HS USB simulation on the i.MX RT and Kinetis K66 (which has more or less the same USB controller) https://youtu.be/3irORtbc4e0

Regards

Mark

 

元の投稿で解決策を見る

2 返答(返信)
1,660件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The HS USBs can be used as device or host (and change between the two roles via OTG protocol). One USB interface can never be used as both host or device at the same time.

On devices with two HS USB controllers one can be host and the other device (or both device or both host).

The following shows dual HS USB simulation on the i.MX RT and Kinetis K66 (which has more or less the same USB controller) https://youtu.be/3irORtbc4e0

Regards

Mark

 

1,644件の閲覧回数
uwe_strempel
Contributor I

Hi Mark,

thank you.

That information helps me alot.

Regards

Uwe

0 件の賞賛
返信