i.MX RT cpu family USB OTG dual role

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT cpu family USB OTG dual role

Jump to solution
930 Views
uwe_strempel
Contributor I

Hi,

can the i.MX RT cpu family (106x/105x/117x etc.) run usb otg dual role (host/device) at same time?

Best regards

Uwe

0 Kudos
Reply
1 Solution
922 Views
mjbcswitzerland
Specialist V

Hi

The HS USBs can be used as device or host (and change between the two roles via OTG protocol). One USB interface can never be used as both host or device at the same time.

On devices with two HS USB controllers one can be host and the other device (or both device or both host).

The following shows dual HS USB simulation on the i.MX RT and Kinetis K66 (which has more or less the same USB controller) https://youtu.be/3irORtbc4e0

Regards

Mark

 

View solution in original post

2 Replies
923 Views
mjbcswitzerland
Specialist V

Hi

The HS USBs can be used as device or host (and change between the two roles via OTG protocol). One USB interface can never be used as both host or device at the same time.

On devices with two HS USB controllers one can be host and the other device (or both device or both host).

The following shows dual HS USB simulation on the i.MX RT and Kinetis K66 (which has more or less the same USB controller) https://youtu.be/3irORtbc4e0

Regards

Mark

 

907 Views
uwe_strempel
Contributor I

Hi Mark,

thank you.

That information helps me alot.

Regards

Uwe

0 Kudos
Reply