flexio_spi_edma example doesn't work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

flexio_spi_edma example doesn't work

1,145 次查看
alexanderhaenel
Contributor I

Hi everyone,

I would like to test the "flexio_spi_edma_lpspi_transfer_slave" example and it does not work.

We had setup the board (IMXRT1050-EVKB Rev: A1) correctly by removing the R334 resisitor and changing R278,R279,R280 and R281 to 0 Ohm.

The needed connection from J24 to SW5 was also done.

To verify the board settings, I can execute the example "flexio_spi_int_lpspi_transfer_slave", and it works fine.

But if the edma example is started, the slave will never finish.

We are waiting at this code position because the isSlaveTransferCompleted is false and the isMasterTransferCompleted is true.

 /* Wait slave received all data. */
    while (!(isSlaveTransferCompleted && isMasterTransferCompleted))
    {
    }

Wenn I look in the slaveRxBuffer I see:

slaveRxData[0] = 0; <- this is wrong

slaveRxData[1] = 0;

slaveRxData[2] = 1;

slaveRxData[3] = 2;

I think this is the problem. The slave can't read der correct transfer size. We miss the first bytes and the slave is never finished.

What can I do to get the edma example to work?

Best regards

Alexander

标签 (1)
0 项奖励
回复
1 回复

1,068 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hello Alexander,

First of all, sorry for the later reply.

Could you help to provide the MCUXpresso SDK version info for EVKB-IMXRT1050?

I checked the latest MCUXpresso SDK version for RT1050 is REV.2.6.1. released at July 3rd 2019.

Thanks for the attention.

best regards,

Mike

0 项奖励
回复