cannot find OTFAD test code for imxRT1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cannot find OTFAD test code for imxRT1170

Jump to solution
2,998 Views
benoit_gonzalv1
Contributor I

Hi,

in the AN13198 document, in section 3.2, it looks that there is a "evkmimxrt1170_flexspi_OTFAD_performance_cm7" test application code. But i can't find it neither in the SDK, nor in the pdf attachement.

Do i miss something ?

Thank you

0 Kudos
Reply
1 Solution
2,991 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please download the demo code via the below link.
https://www.nxp.com.cn/docs/en/application-note-software/AN13198SW.zip
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,777 Views
eforzano
Contributor II

Hi! 

The link to OTFAD example is a dead link. Is there another link to it? I am looking for an OTFAD example for our open source MCUbootloader. 

Also, in the SDK it seems someone left out OTFAD as a feature/driver for 117X examples, that probably needs to be fixed because it doesn't include the files by default. 

Thanks,
Ernie


0 Kudos
Reply
2,992 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please download the demo code via the below link.
https://www.nxp.com.cn/docs/en/application-note-software/AN13198SW.zip
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,763 Views
vishnusudhankj
Contributor III

Hi @jeremyzhou 

Is there any sample program available to check the IEE XiP encryption performance?

 

 

0 Kudos
Reply
2,751 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @vishnusudhankj ,

There's no related demo code until now.

BR,

Jeremy

0 Kudos
Reply