cannot find OTFAD test code for imxRT1170

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cannot find OTFAD test code for imxRT1170

ソリューションへジャンプ
3,087件の閲覧回数
benoit_gonzalv1
Contributor I

Hi,

in the AN13198 document, in section 3.2, it looks that there is a "evkmimxrt1170_flexspi_OTFAD_performance_cm7" test application code. But i can't find it neither in the SDK, nor in the pdf attachement.

Do i miss something ?

Thank you

0 件の賞賛
返信
1 解決策
3,080件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please download the demo code via the below link.
https://www.nxp.com.cn/docs/en/application-note-software/AN13198SW.zip
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,866件の閲覧回数
eforzano
Contributor II

Hi! 

The link to OTFAD example is a dead link. Is there another link to it? I am looking for an OTFAD example for our open source MCUbootloader. 

Also, in the SDK it seems someone left out OTFAD as a feature/driver for 117X examples, that probably needs to be fixed because it doesn't include the files by default. 

Thanks,
Ernie


0 件の賞賛
返信
3,081件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please download the demo code via the below link.
https://www.nxp.com.cn/docs/en/application-note-software/AN13198SW.zip
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,852件の閲覧回数
vishnusudhankj
Contributor III

Hi @jeremyzhou 

Is there any sample program available to check the IEE XiP encryption performance?

 

 

0 件の賞賛
返信
2,840件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @vishnusudhankj ,

There's no related demo code until now.

BR,

Jeremy

0 件の賞賛
返信