cannot find OTFAD test code for imxRT1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

cannot find OTFAD test code for imxRT1170

跳至解决方案
2,982 次查看
benoit_gonzalv1
Contributor I

Hi,

in the AN13198 document, in section 3.2, it looks that there is a "evkmimxrt1170_flexspi_OTFAD_performance_cm7" test application code. But i can't find it neither in the SDK, nor in the pdf attachement.

Do i miss something ?

Thank you

0 项奖励
回复
1 解答
2,975 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please download the demo code via the below link.
https://www.nxp.com.cn/docs/en/application-note-software/AN13198SW.zip
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
1,761 次查看
eforzano
Contributor II

Hi! 

The link to OTFAD example is a dead link. Is there another link to it? I am looking for an OTFAD example for our open source MCUbootloader. 

Also, in the SDK it seems someone left out OTFAD as a feature/driver for 117X examples, that probably needs to be fixed because it doesn't include the files by default. 

Thanks,
Ernie


0 项奖励
回复
2,976 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Please download the demo code via the below link.
https://www.nxp.com.cn/docs/en/application-note-software/AN13198SW.zip
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
2,747 次查看
vishnusudhankj
Contributor III

Hi @jeremyzhou 

Is there any sample program available to check the IEE XiP encryption performance?

 

 

0 项奖励
回复
2,735 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi @vishnusudhankj ,

There's no related demo code until now.

BR,

Jeremy

0 项奖励
回复