boot from USB disk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

boot from USB disk

2,661 Views
calvin1
Contributor II

Hi,

I read the manual "i.MX MCU Manufacturing User's Guide", in the appendix, it mentioned that Plugin boot application is able to boot from USB Disk, I wonder if this is also supported on iMXRT1010EVK, what are necessary steps to make it?

Labels (1)
0 Kudos
Reply
1 Reply

2,576 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Calvin Lin,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
The Plugin feature is supported, however, we don't recommend the customer to implement it, as it's a bit complicated.
I've attached a i.MX MCU Manufacturing User's Guide which demonstrates an example of a Plugin boot application can give you some inspirations.

Have a great day.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply