Using xbar with timer to generate PWM signal on iMXRT1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using xbar with timer to generate PWM signal on iMXRT1050

1,525 Views
davidouatt08
Contributor I

Hello,

I'm using iMXRT1050 and need to generate a PWM signal on pin GPIO_B1_03, mapped to XBAR1_XBAR_INOUT17 (TMR3, TIMER_OUTPUT,0). 

Can't find any example in SDK2.5 (MCUXpresso).

Somebody already done this with iMXRT?

Regards

0 Kudos
Reply
1 Reply

1,334 Views
jeremyzhou
NXP Employee
NXP Employee

Hi David OUATTARA,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To implement the application, I think you need to do some modifications to the xbara demo.
If you have any further questions, please feel free to contact me.

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply