Understanding bin format

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Understanding bin format

1,715 Views
rans
Senior Contributor I

Hello,

When need to copy bin file to a storage device (RAM or flash depends on linker configuration),

Is it only required that we copy the .bin format into the start address of text ? (which is the text start address)

Or does bin format also contains data that need to be written into another start address ? I

Thank you,

ranran

0 Kudos
Reply
1 Reply

1,630 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

   In general, it depends on ...

Often .bin file is just memory image without any structure and headers. 

What file do You mean? What is problem environment? 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply