Understanding bin format

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Understanding bin format

1,720件の閲覧回数
rans
Senior Contributor I

Hello,

When need to copy bin file to a storage device (RAM or flash depends on linker configuration),

Is it only required that we copy the .bin format into the start address of text ? (which is the text start address)

Or does bin format also contains data that need to be written into another start address ? I

Thank you,

ranran

0 件の賞賛
返信
1 返信

1,635件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   In general, it depends on ...

Often .bin file is just memory image without any structure and headers. 

What file do You mean? What is problem environment? 

 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 件の賞賛
返信