USB recognition error on uClinux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB recognition error on uClinux

3,456件の閲覧回数
minkyu_shon
Contributor I

Hi.

i.MXRT 1060-EVK based board is under review.

 With the following : 

USB_waveform.png

There are cases when USB is recognized and not. There is a difference in the D+ waveform,

but I want to know the reason for the other part....

The circuit is as follows.

USB_Circuit.png

I'd like you to tell me if there is a problem...

Thanks.....

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,314件の閲覧回数
minkyu_shon
Contributor I

Hi. Victor....

A Linux (uClinux) Board Support Package is running fine.

booting_picture.png

If you look at the log above, boot is working fine.

Regards,
Shon.

0 件の賞賛
返信

3,314件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Shon, 

Unfortunately, this board support package is from a third-party provider. I recommend contacting their support line, as they will be able to provide correct information.

If you would like to try our examples please download the SDK. There are several USB examples that can get you started. 
Best Regards, 
Victor 
0 件の賞賛
返信

3,314件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hi SON MINKYU, 

The circuit looks fine. Are you running a Linux (uClinux) Board Support package on your board? 

Regards, 

Victor 

0 件の賞賛
返信