USB host example code for mimxrt1170-evk not working as expected.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB host example code for mimxrt1170-evk not working as expected.

2,991 次查看
Shehan_Janidu
Contributor III

I loaded the example code given to connect USB virtual printer. The code compiles properly giving no errors. But when the code is loaded, the expected functionality doesn't take place. The overview of the full example project and expected functionality is explained in the attached pdf. 

The example project name is "dev_printer_virtual_text_bm_cm7"

The project can be accessed through following link  Link to project 

iMXRT1170     

0 项奖励
回复
4 回复数

2,971 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Shehan_Janidu,

I believe this is a duplicated post from the following link: https://community.nxp.com/t5/i-MX-RT/USB-host-example-code-for-mimxrt1170-evk-not-working-properly/t...

If it is ok with you, I will continue supporting on that other post in order to prevent double efforts.

BR,
Edwin.

0 项奖励
回复

2,963 次查看
Shehan_Janidu
Contributor III

I found the solution for the post you are referring.
Yes this post is about the same code but different issue. I only need your support for this particular post @EdwinHz 

More specifically the problem I have is, according to the documentation given, a software should installed automatically after running the code. But when I am running the code, the expected software does not get installed. Thats problem now I am dealing with. iMXRT1170 

0 项奖励
回复

2,925 次查看
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Shehan_Janidu,

You should be able to install the driver manually by following this community post: https://community.nxp.com/t5/Kinetis-Microcontrollers/quot-MCU-VIRTUAL-COM-DEMO-quot-and-demo-app-fo...

Rather than using the path specified by that post, however, you would use the following:

"<SDK installation root>\SDK_2_14_0_MIMXRT1170-EVKB.zip\middleware\usb"

By default, the SDK installation root is:

"C:\Users\<user>\mcuxpresso\02\SDKPackages"

 

I hope this helps,
Edwin,

0 项奖励
回复

2,875 次查看
Shehan_Janidu
Contributor III

I ran the code again and followed following steps,

      in device manager following icons were displayed,

                           usb 1.png

 

After that I updated the drivers both ways, manually and by clicking on "let me pick"

usb 2.png

But even after doing that, still generic printer is not shown in the printer section,

usb 3.png

And when I go to devices and printers folder, it shows like this,

usb 4.png

Can u suggest what can I do to fix this issue. In addition I have a doubt to clear out. The printing process that we going to do here is fully virtual one instead of physical one. Am I right ?

@EdwinHz  iMXRT1170 

0 项奖励
回复