USB CDC Driver Re-Certification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB CDC Driver Re-Certification

跳至解决方案
4,467 次查看
dh1
Contributor II

Hello

We are using CDC Class driver for our NXP RT MCU.

Now we would like to use our NXP-Assigned PID with the driver provided by NXP with the SDK. This is the fsl_ucwxp.inf file with the cdc.cat file.

First question: Is this driver certified by Microsoft?

To use this driver with our own PID, and to give a proper name in the device manager, we need to edit the .inf file. This will void the certification of the driver.
To alllow driver installation at customers without security warning, we need to re-certify the driver by Microsoft. To be able to do this, NXP will need to confirm to Microsoft that we are allowed to do this.

Is this allowed by NXP and has it been done before?

Thanks and regards,
Daniel

0 项奖励
回复
1 解答
4,450 次查看
jingpan
NXP TechSupport
NXP TechSupport
0 项奖励
回复
4 回复数
4,440 次查看
mjbcswitzerland
Specialist V

Hi @jingpan 

Interestingly in the link that you show it points out that the NXP VID/PID program can't be used for i.MX RT parts - it is only valid for Cortex M LPC and Kinetis based products and Cortex-A based i.MX application processors.

Is that really the case?

Regards

Mark

 

0 项奖励
回复
4,410 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @mjbcswitzerland ,

No, it can used on i.mxRT. The last update of this post is 07-15-2016. RT wasn't announced at that time.

 

Regards,

Jing

标记 (1)
0 项奖励
回复
4,401 次查看
mjbcswitzerland
Specialist V

Hi

Many thanks! That is very good to know!

Regards

Mark

 

0 项奖励
回复
4,451 次查看
jingpan
NXP TechSupport
NXP TechSupport
0 项奖励
回复