Trace is impossible on iMXRT1021 with Ethernet and QSPI !

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trace is impossible on iMXRT1021 with Ethernet and QSPI !

1,457件の閲覧回数
chriscowdery
Contributor V

I'm going to put this out there - I'm very frustrated with the design of the iMXRT1021.

Specifically, the pin multiplexing options are very poorly designed.

My use case is what I would expect to be very common for a processor of this class. I require Ethernet connectivity, and the lowest cost external Flash. This means my Flash is QSPI. I am sure many other designs are similar.

I also run FreeRTOS, which means debugging can be very complex.

I have discovered that with my combination, it is IMPOSSIBLE to use the ARM Embedded Trace Module for Debug !

This is for two reasons:

  1. The pin multiplexer allows only 2 of these peripherals to be used at the same time: TRACE, ENET and FlexSPI_A
  2. There is no ETB. So data from the ETM cannot be stored on-chip and output slowly via SWO. SWO can only sample the Program Counter for profiling, it is not fast enough for Instruction Trace.

The documentation is extremely poor in this regard, for example, the TRACE pins do not appear in the Reference Manual chapter 9 "External Signals and Pin Multiplexing". They are instead listed separately in chapter 27 "ARM Cortex M7 Platform". And nowhere is there an overall description of what debugging options are available on this part, their limitations, how to use etc. There are instead a number of separate remarks, often referring to ARM documentation.

Please forgive my obvious frustration here, but I cannot help but think that the debug infrastructure on this part is badly designed, and hidden behind bad documentation. This translates into many hours and days of wasted time to understand the situation and discover the best debug features are not accessible!

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 返信

1,407件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Chris Cowdery,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'm sorry to hear your frustration, however regarding your application, maybe you can try to utilize some functionalities included in MCUXpresso IDE to assist in debugging applications built around FreeRTOS. It provides another way to debug and trace the FreeRTOS demo project.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信