Hi Manuel,
Is this a limitation of RT1010 only?
This is a limitation of the FlexIO module not of the RT.
For instance, does the K80 kinetics series FlexIO have the same limitation? (I don't think so but want to check with NXP)
The FlexIO module on the RT families was inherited from the Kinetis families, so this limitation of the module is also present in these families.
Is there any plan to have a new silicon release that fix this limitation?
As mentioned in the first question, this is not a limitation of the RT but the module. So, there aren't any plans to "fix" this limitation on future releases of the RT.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct"button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------