TCM & Cache...

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,664件の閲覧回数
EdSutter
Senior Contributor II

I'm working on a new feature (SPEEX echo cancellation) for my hardware that, as of right now, is not working because of what appears to be not-enough-horsepower in the '1062.  Its still pretty early, so its possible (i.e. likely) I just have a problem with how I'm using the echo canceller, but it raises a general question that I'm sure has already been answered somewhere regarding optimization...

I have text and data mapped to ITCM and DTCM respectively, so does it matter how I have cache configured (MPU) for those areas? Is cache even in the picture when using TCM?  

tx

Ed

0 件の賞賛
返信
1 解決策
2,659件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The tightly coupled memeries operate at core speed without wait states and are not cacheable.

Regards

Mark

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,654件の閲覧回数
EdSutter
Senior Contributor II

That's what I thought...

Thanks Mark

0 件の賞賛
返信
2,660件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The tightly coupled memeries operate at core speed without wait states and are not cacheable.

Regards

Mark

 

0 件の賞賛
返信