TCM & Cache...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TCM & Cache...

跳至解决方案
1,795 次查看
EdSutter
Senior Contributor II

I'm working on a new feature (SPEEX echo cancellation) for my hardware that, as of right now, is not working because of what appears to be not-enough-horsepower in the '1062.  Its still pretty early, so its possible (i.e. likely) I just have a problem with how I'm using the echo canceller, but it raises a general question that I'm sure has already been answered somewhere regarding optimization...

I have text and data mapped to ITCM and DTCM respectively, so does it matter how I have cache configured (MPU) for those areas? Is cache even in the picture when using TCM?  

tx

Ed

0 项奖励
回复
1 解答
1,790 次查看
mjbcswitzerland
Specialist V

Hi

The tightly coupled memeries operate at core speed without wait states and are not cacheable.

Regards

Mark

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,785 次查看
EdSutter
Senior Contributor II

That's what I thought...

Thanks Mark

0 项奖励
回复
1,791 次查看
mjbcswitzerland
Specialist V

Hi

The tightly coupled memeries operate at core speed without wait states and are not cacheable.

Regards

Mark

 

0 项奖励
回复