Hi,
With "Link Application to RAM" setting, When board is power off and on then my application doesn't run. So this setting doesn't work for me.
Our board has external QSPI Flash to store the code image. During power on BootROM should copy code image from flash to ITCM RAM.
I am using dual cores CM7, CM4 in project. CM4 anyway runs in its RAM(ITCM_CM4). But i am looking for CM7 code, should also be executed from ITCM_CM7.
Please suggest.
Is there Flash Loader for IMXRT1175, if any kindly provide the link for Flash Loader of IMXRT1175.
Thanks in advance,
Pavani.