Hello,
I followed the document "I.MX RT - How to Boot to SDRAM" from the i.MX RT Knowledge Base but can't get it working.
Hardware:
Embedded Artists i.MX RT1064 uCOM (SDRAM 32 MB)
Segger JLink Plus
Software:
MCUXpresso 11.9.1_2170
What I did:
I linked the Hello World application from the SDK to the SDRAM.
I enabled the DCD header (XIP_BOOT_HEADER_DCD_ENABLE=1).
Looking at the memory map, it seems we have everything we need:
.boot_hdr 0x80000000 0x2000
FILL mask 0xff
0x80000000 __boot_hdr_start__ = ABSOLUTE (.)
*(SORT_BY_ALIGNMENT(.boot_hdr.conf))
.boot_hdr.conf
0x80000000 0x200 ./xip/evkmimxrt1064_flexspi_nor_config.o
0x80000000 qspiflash_config
0x00001000 . = 0x1000
*fill* 0x80000200 0xe00 ff
*(SORT_BY_ALIGNMENT(.boot_hdr.ivt))
.boot_hdr.ivt 0x80001000 0x20 ./xip/fsl_flexspi_nor_boot.o
0x80001000 image_vector_table
0x00001020 . = 0x1020
*(SORT_BY_ALIGNMENT(.boot_hdr.boot_data))
.boot_hdr.boot_data
0x80001020 0x10 ./xip/fsl_flexspi_nor_boot.o
0x80001020 g_boot_data
0x00001030 . = 0x1030
*(SORT_BY_ALIGNMENT(.boot_hdr.dcd_data))
.boot_hdr.dcd_data
0x80001030 0x410 ./board/dcd.o
0x80001030 dcd_data
0x80001440 __boot_hdr_end__ = ABSOLUTE (.)
0x00002000 . = 0x2000
*fill* 0x80001440 0xbc0 ff
.text 0x80002000 0x4f68
FILL mask 0xff
0x80002000 __vectors_start__ = ABSOLUTE (.)
*(SORT_BY_ALIGNMENT(.isr_vector))
.isr_vector 0x80002000 0x2b8 ./startup/startup_mimxrt1064.o
0x80002000 __Vectors
0x80002000 g_pfnVectors
0x800022b8 . = ALIGN (0x4)
0x800022b8 __section_table_start = .
0x800022b8 __data_section_table = .
Finally, I generated a bin file and flashed it to 0x70000000.
jlink log:
Executing flash operation 'Program' (Program executable into flash eaimxrt1064_hello_world_sdram.bin) - Wed Jun 12 08:55:41 CEST 2024
Checking MCU info...
Scanning for targets...
Executing flash action...
SEGGER J-Link Commander V7.96c (Compiled Apr 2 2024 12:36:46)
DLL version V7.96c, compiled Apr 2 2024 12:36:21
J-Link Command File read successfully.
Processing script file...
J-Link>ExitOnError 1
J-Link Commander will now exit on Error
J-Link>r
J-Link connection not established yet but required for command.
Connecting to J-Link via USB...O.K.
Firmware: J-Link V11 compiled Mar 14 2024 13:16:08
Hardware version: V11.00
J-Link uptime (since boot): 0d 00h 44m 27s
S/N: 851006059
License(s): RDI, FlashBP, FlashDL, JFlash, GDB
USB speed mode: High speed (480 MBit/s)
VTref=3.305V
Target connection not established yet but required for command.
Device "MIMXRT1064XXX6A" selected.
Connecting to target via SWD
InitTarget() start
InitTarget() end - Took 1.14ms
Found SW-DP with ID 0x0BD11477
Failed to power up DAP
InitTarget() start
InitTarget() end - Took 1.27ms
Found SW-DP with ID 0x0BD11477
DPIDR: 0x0BD11477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[1]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x04770041)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FD000
CPUID register: 0x411FC271. Implementer code: 0x41 (ARM)
Cache: L1 I/D-cache present
Found Cortex-M7 r1p1, Little endian.
FPUnit: 8 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ E00FD000
[0][0]: E00FE000 CID B105100D PID 000BB4C8 ROM Table
ROMTbl[1] @ E00FE000
[1][0]: E00FF000 CID B105100D PID 000BB4C7 ROM Table
ROMTbl[2] @ E00FF000
[2][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
[2][1]: E0001000 CID B105E00D PID 000BB002 DWT
[2][2]: E0002000 CID B105E00D PID 000BB00E FPB-M7
[2][3]: E0000000 CID B105E00D PID 000BB001 ITM
[1][1]: E0041000 CID B105900D PID 001BB975 ETM-M7
[1][2]: E0042000 CID B105900D PID 004BB906 CTI
[0][1]: E0040000 CID B105900D PID 000BB9A9 TPIU-M7
[0][2]: E0043000 CID B105F00D PID 001BB101 TSG
I-Cache L1: 32 KB, 512 Sets, 32 Bytes/Line, 2-Way
D-Cache L1: 32 KB, 256 Sets, 32 Bytes/Line, 4-Way
Memory zones:
"Default" Description: Default access mode
Cortex-M7 identified.
Reset delay: 0 ms
Reset type NORMAL: Resets core & peripherals via SYSRESETREQ & VECTRESET bit.
ResetTarget() start
Could not find valid reset vector.
Target halted on flash header read.
ResetTarget() end - Took 124ms
AfterResetTarget() start
AfterResetTarget() end - Took 1.44ms
J-Link>h
PC = 002114C8, CycleCnt = 00000000
R0 = 00000001, R1 = 402A4210, R2 = 5AF05AF0, R3 = 00000004
R4 = 00000001, R5 = 0021B368, R6 = 00000000, R7 = 401F46E0
R8 = 00000000, R9 = 00000000, R10= 41EDA67B, R11= 400F8000
R12= 00000000
SP(R13)= 20200D10, MSP= 20200D10, PSP= 00000000, R14(LR) = 0020F8FF
XPSR = 41000000: APSR = nZcvq, EPSR = 01000000, IPSR = 000 (NoException)
CFBP = 00000000, CONTROL = 00, FAULTMASK = 00, BASEPRI = 00, PRIMASK = 00
FPS0 = 00000000, FPS1 = 00000000, FPS2 = 00000000, FPS3 = 00000000
FPS4 = 00000000, FPS5 = 00000000, FPS6 = 00000000, FPS7 = 00000000
FPS8 = 00000000, FPS9 = 00000000, FPS10= 00000000, FPS11= 00000000
FPS12= 00000000, FPS13= 00000000, FPS14= 00000000, FPS15= FFFFFFFF
FPS16= 00000000, FPS17= 00000000, FPS18= 00000000, FPS19= 00000000
FPS20= 00000000, FPS21= 00000000, FPS22= 00000000, FPS23= 00000000
FPS24= 00000000, FPS25= 00000000, FPS26= 00000000, FPS27= 00000000
FPS28= 00000000, FPS29= 00000000, FPS30= 00000000, FPS31= FFFFFFFF
FPSCR= 00000000
J-Link>loadfile "/home/mn/Documents/MCUXpresso_11.9.1_2170/workspace/eaimxrt1064_hello_world_sdram/Debug/eaimxrt1064_hello_world_sdram.bin" 0x70000000
'loadfile': Performing implicit reset & halt of MCU.
ResetTarget() start
Could not find valid reset vector.
Target halted on flash header read.
ResetTarget() end - Took 123ms
AfterResetTarget() start
AfterResetTarget() end - Took 2.08ms
Downloading file [/home/mn/Documents/MCUXpresso_11.9.1_2170/workspace/eaimxrt1064_hello_world_sdram/Debug/eaimxrt1064_hello_world_sdram.bin]...
J-Link: Flash download: Bank 0 @ 0x70000000: Skipped. Contents already match
O.K.
J-Link>qc
Script processing completed.
In the tutorial, an s19 file is generated, but I didn't succeed in flashing this file to the flash memory (as it's linked to SDRAM, the JLink tries to flash it to SDRAM, which is not what I want).
After all this, I see that the application doesn't start. Moreover, in the JLink log, you can see "Could not find valid reset vector."
What am I doing wrong?
Thank you,
Michael