Simulation models for I.MX RT633 I3C interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simulation models for I.MX RT633 I3C interface

1,872件の閲覧回数
shaozhongliangs
NXP Employee
NXP Employee

  Customer is evaluating RT633 I3C in chassis managment system.  Customer needs the I3C  simulation model for testing the reaction of the I3C about how it works in detail.

   I had provided the BSDL(Boundary Scan Description Language) and IBIS model files to customer. But customer told me that there wasn't I3C simulation model in these files.

  Is there an official I3C master simulation model for customer's verifying design? 

RT600 Models in NXP website:

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/i-mx-rt-crossover-...

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,141件の閲覧回数
jacobvecht
Contributor III

The RT633 is as real as the Tooth Fairy! It simply does not exist, and references to it have now been removed from the NXP website and from the RT600 data sheet. 

0 件の賞賛
返信

1,855件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there an official I3C master simulation model for customer's verifying design?
-- No, I'm afraid that NXP doesn't have a similar kind of simulation model.
Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信