SRAM memory reserving

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SRAM memory reserving

ソリューションへジャンプ
4,514件の閲覧回数
vijayc1
Contributor II

Hai im using IMXRT1062 ,i need to reserve SRAM memory of 4kb how to do that and how to read and write on SRAM memory location?

0 件の賞賛
返信
1 解決策
4,494件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @vijayc1 

   In the linker file, define a ram memory range for your own user ram area, then you define the variable in that range, after reset, no power off, the data still exists, you can read back the RAM data after reset.

 

Wish it helps you!

Best Regards,

Kerry

   

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
4,505件の閲覧回数
vijayc1
Contributor II

hai kerry i need it on RT1062 internal RAM.

0 件の賞賛
返信
4,501件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @vijayc1 ,

  If you need to use the internal ram, it is more easy, internal RAM contains: 128K ITCM,128k DTCM, 256k OCRAM. different RAM in the different location.

  About the operation, you just need to operate the related address is OK.

  Which IDE you are using? 

  If mcuxpresso, you can refer to this post to use the related address:

https://community.nxp.com/docs/DOC-335283

 

Wish it helps you!

Best Regards,

Kerry

0 件の賞賛
返信
4,498件の閲覧回数
vijayc1
Contributor II

I am using an application code where i need to write an value at a particular location of internal RAM to do a soft restart is that possible? because i need to read that value back again in the bootloader after the soft restart.

0 件の賞賛
返信
4,497件の閲覧回数
vijayc1
Contributor II

also can you suggest me if there are any particular registers that wont get erased after an reboot?

0 件の賞賛
返信
4,495件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @vijayc1 

   In the linker file, define a ram memory range for your own user ram area, then you define the variable in that range, after reset, no power off, the data still exists, you can read back the RAM data after reset.

 

Wish it helps you!

Best Regards,

Kerry

   

0 件の賞賛
返信
4,474件の閲覧回数
vijayc1
Contributor II

thank you for the reply,is there any code snippet to do the software reset?

0 件の賞賛
返信
4,508件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @vijayc1 

   The SRAM you mentioned is the external SRAM chip or the RT1062 internal RAM?

   If it is the external SRAM chip, you need to use the SEMC to connect to your external SRAM, you can refer to the SDRAM code, it will remap to the 0x80000000 address, you need to initialize the SEMC with your external memory, then you can access the related address directly.

  SDK code:

SDK_2_10_0_EVK-MIMXRT1060\boards\evkmimxrt1060\driver_examples\semc\sdram

Wish it helps you!

Best Regards,

Kerry

0 件の賞賛
返信