SAI MSB First Field

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SAI MSB First Field

跳至解决方案
4,045 次查看
amwilhite
Contributor III

I was hoping someone could explain the effect of the SAI MSB First (MF) field on the receipt of data via I2S.

In this case, does MSB still stand for most significant byte (and not most significant bit)?

My interpretation is the following:

MSB First (MF) specifies if the first byte received per word is the most significant or least significant.

Example:

16-bit words

1111 0000 0000 1111 is shifted out, from left to right

With the MSB First (MF) set to 1 (selecting MSB):

The sample value is 0xF00F

the receive buffer (in our little-endian system) reads:

Base Address: 0x0F

Base Address + 1: 0xF0

With the LSB First (MF) set to 0 (selecting LSB):

The sample value is 0x0FF0

The receive buffer  (in our little-endian system) reads:

Base Address: 0xF0

Base Address + 1: 0x0F

Is this correct?

0 项奖励
回复
1 解答
3,952 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Austin Wilhite,

   You can check the RT reference manual about Figures 37-2 and 37-3, it means the Data in the FIFO can be aligned anywhere within the 32-bit wide register through the use of the First Bit Shifted configuration field, which selects the bit index (between 31 and 0) of the first bit shifted.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,716 次查看
vdinh
Contributor I

Can you explain how to interpret Figures 37-2 and 37-3? It's not clear to me what exactly they are attempting to illustrate.

0 项奖励
回复
3,952 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Austin Wilhite ,

    After double check with our SAI expert, the MSB and LSB is significant bit, not byte.

   The RT SAI in default is using LSB.

   When you use the FIFO aligned within the 32bit wide register, you need to refer to this Figure:

pastedImage_2.png

Wish it helps you!

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,952 次查看
amwilhite
Contributor III

Kerry,

Although the RT SAI registers default to LSb, the SAI driver defaults to MSb.

Can you explain how to interpret Figures 37-2 and 37-3? It's not clear to me what exactly they are attempting to illustrate.

0 项奖励
回复
3,953 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Austin Wilhite,

   You can check the RT reference manual about Figures 37-2 and 37-3, it means the Data in the FIFO can be aligned anywhere within the 32-bit wide register through the use of the First Bit Shifted configuration field, which selects the bit index (between 31 and 0) of the first bit shifted.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复