i.MXRT1052 Power-up circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MXRT1052 Power-up circuit

841 Views
mail3
Contributor I

I have one version of PCB that is based on i.MXRT1052. It is not meet a suitable connection for the power-up sequence. Therefore the first version of PCB did not work.

Now, I have added an R-C circuit as described in the hardware design guide. I have attached the schema.

Is it a suitable connection for programming the MCU?

0 Kudos
Reply
1 Reply

834 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is it a suitable connection for programming the MCU?
-- Yes, I think so.
Have a great day.
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply