Recommended decoupling RT1064?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recommended decoupling RT1064?

Jump to solution
2,981 Views
carstengroen
Senior Contributor II

In the RT1050/RT1060 Hardware Development Guide: https://www.nxp.com/docs/en/user-guide/MIMXRT105060HDUG.pdf 

on page 3 is a list of the various power connections and the recommended decoupling capacitors. For Pin VDD_SNVS_CAP is listed 1 x 0.22uF and 1 x 4.7uF:

pastedImage_4.png

On the other hand, when looking at the EVK schematics for the 1064EVK, only a single 0.22uF capactor is shown:

pastedImage_3.png

Which one is "the most recommended" way ?

Also, the NVCC_PLL signal is not mentioned in the Hardware Development Guide, according to the EVK, there is a single 0.22uF and a single 4.7uF as decoupling, I assume this is the recommended way ?

1 Solution
2,836 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

There is single 0.22uF + a single 4.7uF or single  0.22uF is ok for the VDD_SNVS_CAP/NVCC_PLL . Hope it help you.

regards

Tina

View solution in original post

2 Replies
2,837 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

There is single 0.22uF + a single 4.7uF or single  0.22uF is ok for the VDD_SNVS_CAP/NVCC_PLL . Hope it help you.

regards

Tina

2,836 Views
carstengroen
Senior Contributor II

Thanks,

I was just confused that there was differences between the EVK and the Hardware Development Guide.

0 Kudos
Reply