Recommend a RT device that supports 2-channel camera input and display at same time

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Recommend a RT device that supports 2-channel camera input and display at same time

1,027 次查看
Jack-Cha
Contributor V

Hi 

Could you please recommend a RT device that supports 2-channel camera input and display at same time?

The application is similart with 2ch-dash cam.

Regards, 

Jack

0 项奖励
回复
1 回复

1,020 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Jack-Cha ,

  May I consider you want to use two CSI at the same time?

  If yes, we recommend you one use the CSI API, another use the flexIO to simulate the CSI to connect your camera.

  Normal CSI, you can refer to the RT SDK CSI code, flexIO emulate CSI, please refer to this AN:

https://www.nxp.com/docs/en/application-note/AN12686.pdf

https://www.nxp.com/docs/en/application-note-software/AN12686SW.zip

 

Wish it helps you!

Best Regards,

Kerry