Recommend a RT device that supports 2-channel camera input and display at same time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recommend a RT device that supports 2-channel camera input and display at same time

1,025件の閲覧回数
Jack-Cha
Contributor V

Hi 

Could you please recommend a RT device that supports 2-channel camera input and display at same time?

The application is similart with 2ch-dash cam.

Regards, 

Jack

0 件の賞賛
返信
1 返信

1,018件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @Jack-Cha ,

  May I consider you want to use two CSI at the same time?

  If yes, we recommend you one use the CSI API, another use the flexIO to simulate the CSI to connect your camera.

  Normal CSI, you can refer to the RT SDK CSI code, flexIO emulate CSI, please refer to this AN:

https://www.nxp.com/docs/en/application-note/AN12686.pdf

https://www.nxp.com/docs/en/application-note-software/AN12686SW.zip

 

Wish it helps you!

Best Regards,

Kerry