RT117x running at maximum performance (1 GHz)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT117x running at maximum performance (1 GHz)

1,891件の閲覧回数
shai_b
Senior Contributor II

Dear Team,

My customer would like to increase the performance of our iMXRT1170 to the maximum.

Can you please guide us on how to achieve that using the EVK?

Waiting for your kind feedback, many thanks.

Regards,

Shai

タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,847件の閲覧回数
lucas_cao
NXP Employee
NXP Employee

The default SDK demo code should work at 1Ghz.

1,851件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

This Application note might be helpful: AN12437: i.MX RT Series Performance Optimization – Application Note (nxp.com)

Additionally, to reach that frequency on the consumer-grade product it is important that the voltage is on overdrive(1.1V - 1.15V) and enable FBB. You might want to use Config Tools to enable this frequency.

Best regards,
Omar

1,836件の閲覧回数
shai_b
Senior Contributor II

@Omar_Anguiano, Thanks a lot for your feedback.

I will keep you posted if I need additional support.

Kind regards,

ShaI

0 件の賞賛
返信

1,867件の閲覧回数
shai_b
Senior Contributor II

Hello team,

there is any update?

Kind regards,

Shai

0 件の賞賛
返信