RT117x running at maximum performance (1 GHz)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT117x running at maximum performance (1 GHz)

1,866 Views
shai_b
Senior Contributor II

Dear Team,

My customer would like to increase the performance of our iMXRT1170 to the maximum.

Can you please guide us on how to achieve that using the EVK?

Waiting for your kind feedback, many thanks.

Regards,

Shai

Tags (1)
0 Kudos
Reply
4 Replies

1,822 Views
lucas_cao
NXP Employee
NXP Employee

The default SDK demo code should work at 1Ghz.

1,826 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

This Application note might be helpful: AN12437: i.MX RT Series Performance Optimization – Application Note (nxp.com)

Additionally, to reach that frequency on the consumer-grade product it is important that the voltage is on overdrive(1.1V - 1.15V) and enable FBB. You might want to use Config Tools to enable this frequency.

Best regards,
Omar

1,811 Views
shai_b
Senior Contributor II

@Omar_Anguiano, Thanks a lot for your feedback.

I will keep you posted if I need additional support.

Kind regards,

ShaI

0 Kudos
Reply

1,842 Views
shai_b
Senior Contributor II

Hello team,

there is any update?

Kind regards,

Shai

0 Kudos
Reply