RT1176 FlexRAM ECC enabled by default?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1176 FlexRAM ECC enabled by default?

ソリューションへジャンプ
842件の閲覧回数
Mike_Z
Contributor I

Is the RT1176 FlexRAM ECC enabled by default, or does the user need to intentionally enable it with a set of preload configuration commands? We're using the MiMXRT1170 - EVKB.

We observed this line of code, but unsure what exactly this means. Thanks in advance for any assistance.

#define
FSL_FEATURE_FLEXRAM_HAS_ECC (1)

タグ(3)
0 件の賞賛
返信
1 解決策
818件の閲覧回数
mayliu1
NXP Employee
NXP Employee

Hi @Mike_Z ,

Thank you so much for your interest in our products and for using our community.

Question:

Is the RT1176 FlexRAM ECC enabled by default, or does the user need to intentionally enable it with a set of preload configuration commands? We're using the MiMXRT1170 - EVKB.

Answer:

The RT1176 FlexRAM ECC disabled by default, The user need to intentionally enable it.

Please refer to MIMXRT1170RM chapter 38.7.1.16 OCRAM Pipeline And ECC Enable (PIPE_ECC_EN)

mayliu1_0-1733455875263.png

 

I suggest you can refer to SDK demo "evkbmimxrt1170_mecc_single_error_cm7"

 

 

Best Regards

mayliu

元の投稿で解決策を見る

1 返信
819件の閲覧回数
mayliu1
NXP Employee
NXP Employee

Hi @Mike_Z ,

Thank you so much for your interest in our products and for using our community.

Question:

Is the RT1176 FlexRAM ECC enabled by default, or does the user need to intentionally enable it with a set of preload configuration commands? We're using the MiMXRT1170 - EVKB.

Answer:

The RT1176 FlexRAM ECC disabled by default, The user need to intentionally enable it.

Please refer to MIMXRT1170RM chapter 38.7.1.16 OCRAM Pipeline And ECC Enable (PIPE_ECC_EN)

mayliu1_0-1733455875263.png

 

I suggest you can refer to SDK demo "evkbmimxrt1170_mecc_single_error_cm7"

 

 

Best Regards

mayliu