RT1052的POR引脚的RESET问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1052的POR引脚的RESET问题

Jump to solution
887 Views
FromCH0
Contributor III

尊敬的NXP:

      RT1052是款性价比很高的主控。很高兴有机会用它来开发产品!

      想请教您们复位方面的问题。贵公司RT1052开发板是通过UM803RS来实现对电压监视和复位的。如果用纽扣电池对VDD_SNVY_IN引脚供电,以实现最低的要求的RTC等运行(日期计算功能)。UM803RS需要接VDD_SNVY_IN引脚供电吗?下图中,POR除了初期下拉之后,后续一直是高电平:上电下电时序.png

如果UM803RS不接VDD_SNVY_IN引脚供电,RESET引脚输出状态未知,是否会影响RTC的正常运行?我上网查了些资料,说UM803RS要接VDD_SNVY_IN引脚供电,而且,RESET引脚需要用VDD_SNVY_IN上拉。

Tags (1)
0 Kudos
Reply
1 Solution
824 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @FromCH0 ,

 

复位芯片不需要接VDD_SNVY_IN引脚供电,只有Por_B需要上拉到VDD_SNVY_IN,而且那个上拉电阻可以不贴的,芯片内部有上拉的。详见附件。

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
886 Views
FromCH0
Contributor III

POR原理图.png

这是NXP的RT1052开发板的原理图(POR相关部分)。

0 Kudos
Reply
885 Views
FromCH0
Contributor III

POR原理图.png

0 Kudos
Reply
825 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @FromCH0 ,

 

复位芯片不需要接VDD_SNVY_IN引脚供电,只有Por_B需要上拉到VDD_SNVY_IN,而且那个上拉电阻可以不贴的,芯片内部有上拉的。详见附件。

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
819 Views
FromCH0
Contributor III

谢了

0 Kudos
Reply