RT1050 Flashloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RT1050 Flashloader

1,786 次查看
brli
Contributor III

Hi,

.srec  can't be elftosb.exe transfered to .bin file, following is config and log, could you help to suggest what's problem?

1、This command no success information output:

C:\Users\Diouf.Guo\Downloads\Flashloader_RT1050_1.1\Tools\elftosb\win>elftosb.exe -f imx -V -c ../../bd_file/imx10xx/imx-flexspinor-normal-unsigned.bd -o ivt_RT1052.bin YH-RT1052.srec
Section: 0x0

2、BD Config file:

options {
flags = 0x00;
startAddress = 0x60000000;
ivtOffset = 0x1000;
initialLoadSize = 0x2000;
DCDFilePath = "dcd.bin";
# Note: This is required if the default entrypoint is not the Reset_Handler
# Please set the entryPointAddress to Reset_Handler address
entryPointAddress = 0x60002000;
}

sources {
elfFile = extern(0);
}

section (0)
{
}

3、SDK map file:

.boot_hdr.conf 0x60000000 Section 512 evkbimxrt1050_flexspi_nor_config.o(.boot_hdr.conf)
.boot_hdr.ivt 0x60001000 Section 32 fsl_flexspi_nor_boot.o(.boot_hdr.ivt)
.boot_hdr.boot_data 0x60001020 Section 16 fsl_flexspi_nor_boot.o(.boot_hdr.boot_data)
RESET 0x60002000 Section 1024 startup_mimxrt1052.o(RESET)
.ARM.Collect$$$$00000000 0x60002400 Section 0 entry.o(.ARM.Collect$$$$00000000)
.ARM.Collect$$$$00000003 0x60002400 Section 4 entry4.o(.ARM.Collect$$$$00000003)
.ARM.Collect$$$$00000004 0x60002404 Section 4 entry5.o(.ARM.Collect$$$$00000004)
.ARM.Collect$$$$00000008 0x60002408 Section 0 entry7b.o(.ARM.Collect$$$$00000008)
.ARM.Collect$$$$0000000A 0x60002408 Section 0 entry8b.o(.ARM.Collect$$$$0000000A)
.ARM.Collect$$$$0000000B 0x60002408 Section 8 entry9a.o(.ARM.Collect$$$$0000000B)
.ARM.Collect$$$$0000000D 0x60002410 Section 0 entry10a.o(.ARM.Collect$$$$0000000D)
.ARM.Collect$$$$0000000F 0x60002410 Section 0 entry11a.o(.ARM.Collect$$$$0000000F)
.ARM.Collect$$$$00002714 0x60002410 Section 4 entry4.o(.ARM.Collect$$$$00002714)
__lit__00000000 0x60002410 Data 4 entry4.o(.ARM.Collect$$$$00002714)

Thanks!

Br Li

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,636 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
Please modify the BD file as the AN12108 shows, then give a try again.
https://www.nxp.com/docs/en/application-note/AN12108.pdf

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复