Am I correct in assuming that each rt1064 device is shipped with a unique mac address ?
How can I read this mac address?
(I am developing software using lwip.)
Hi,
Daniel is right, but if You don't have the need for a big MAC address block, the cheaper way is to buy an Serial EEPROM with pre-programmed MAC-Address (see 24AA02E48 or similar).
Martin
Hi
NXP does not supply MAC addresses for its products. The only way, I see, is to buy them from the IEEE:
http://standards.ieee.org/regauth/oui/index.shtml
https://standards.ieee.org/regauth-bin/application?rt=OUI
If you refer to one the lwip examples in the SDK, there is a macro defined the MAC address.
SDK_2.6.1_EVK-MIMXRT1064\boards\evkmimxrt1064\lwip_examples\lwip_ping\freertos
/* MAC address configuration. */
#define configMAC_ADDR \
{ \
0x02, 0x12, 0x13, 0x10, 0x15, 0x11 \
}
Regards
Daniel