Question about Using HyperRam and HyperFlash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about Using HyperRam and HyperFlash

ソリューションへジャンプ
3,444件の閲覧回数
ChekhovMark
Contributor II

Hi, I have some problems developing an I.MX 1052 application. I need more GPIOs, and flash speed is critical. so I'm thinking about using HyperRam and HyperFlash instead of QSPI Flash and SDRAM. Is it posssible to mount both HyperRam and HyperFlash simultaneously on one flexSPI instance, and XIP boot from HyperFlash? If I do so, will the access speed drop when accessing RAM and FLASH together?

Thanks.

ラベル(3)
0 件の賞賛
返信
1 解決策
3,260件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Chekhov Mark,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)  Is it possible to mount both HyperRam and HyperFlash simultaneously on one FlexSPI instance, and XIP boot from HyperFlash?
-- No, I'm afraid not.
For the MIMXRT1052, it's capable of working with the HyperRam and HyperFlash simultaneously, as it has the FlexSPI A and FlexSPI B.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,261件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Chekhov Mark,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)  Is it possible to mount both HyperRam and HyperFlash simultaneously on one FlexSPI instance, and XIP boot from HyperFlash?
-- No, I'm afraid not.
For the MIMXRT1052, it's capable of working with the HyperRam and HyperFlash simultaneously, as it has the FlexSPI A and FlexSPI B.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信